{"words":[["0",""],["300","Hello,"],["660",""],["1020","and"],["1290","welcome"],["1710","to"],["1890","our"],["2100","in-depth"],["2340",""],["2700","look"],["3000","at"],["3150","communications"],["4260","with"],["4470","precision"],["4740",""],["5010","data"],["5340","converters."],["6210",""],["6570","In"],["6870","this"],["7170","video,"],["7535",""],["7900","we"],["8039","describe"],["8309",""],["8580","digital"],["9060","communications"],["10170","and"],["10350","the"],["10440","basics"],["10725",""],["11010","of"],["11160","Serial"],["11415",""],["11670","Peripheral"],["12390","Interface,"],["13170","or"],["13410","SPI"],["13665",""],["13920","communication."],["14990",""],["15480","We'll"],["15750","discuss"],["16020",""],["16290","the"],["16440","communication"],["17310","structure"],["17655",""],["18000","and"],["18390","the"],["18540","required"],["18930",""],["19320","digital"],["19590",""],["19860","lines,"],["20185",""],["20510",""],["20910","then"],["21270","we'll"],["21540","show"],["21840","different"],["22200","modes"],["22560","of"],["22680","SPI"],["23040","communication,"],["24120","and"],["24450","finally"],["24750",""],["25050","give"],["25260","an"],["25350","example"],["25635",""],["25920","of"],["26040","how"],["26310","SPI"],["26700","data"],["27060","is"],["27270","transmitted"],["27930","to"],["28350","and"],["28620","received"],["28890",""],["29160","by"],["29580","a"],["29760","peripheral"],["30390","device."],["30735",""],["31080",""],["31350",""],["31620","Many"],["32040","precision"],["32355",""],["32670","analog"],["32940",""],["33210","devices"],["33540",""],["33870","have"],["34080","a"],["34140","digital"],["34395",""],["34650","interface"],["35310","between"],["35760","a"],["35820","microcontroller,"],["37020","known"],["37350","as"],["37500","a"],["37560","controller,"],["38310","and"],["38610","a"],["38670","controlled"],["39390","device,"],["39705",""],["40020","known"],["40290","as"],["40440","a"],["40500","peripheral."],["41370",""],["41820","Using"],["42300","precision"],["42570","ADCs"],["42840",""],["43215",""],["43590","as"],["43770","an"],["43890","example,"],["44300",""],["44710","the"],["44760","peripheral"],["45570","ADC"],["45870",""],["46170","measures"],["46620","an"],["46780","input"],["47160","voltage,"],["47475",""],["47790","and"],["48120","the"],["48240","controller"],["48840","microcontroller"],["49830","reads"],["50250","the"],["50370","data"],["50700","through"],["50940","digital"],["51420","communications."],["52680",""],["53130","With"],["53400","precision"],["53655",""],["53910","DACs"],["54225","as"],["54540","the"],["54660","second"],["55080","example,"],["55505",""],["55930","the"],["55980","controller"],["56550","microcontroller"],["57450","writes"],["57810","a"],["57900","digital"],["58380","word"],["58680","to"],["58890","the"],["59010","DAC"],["59400","to"],["59520","set"],["59790","an"],["59940","output"],["60390","voltage."],["60750",""],["61110",""],["61440","In"],["61680","both"],["61980","types"],["62370","of"],["62490","devices,"],["62895",""],["63300","this"],["63570","communication"],["64410","may"],["64620","be"],["64800","bidirectional."],["65880",""],["66135",""],["66390","Many"],["66750","precision"],["67020",""],["67290","data"],["67560","converters"],["68160","may"],["68340","require"],["68640",""],["68940","some"],["69240","configuration"],["70260","and"],["70620","programming."],["71610",""],["72030","Digital"],["72510","communications"],["73380","are"],["73500","needed"],["73890","to"],["74010","write"],["74310","to"],["74670","and"],["75060","read"],["75360","from"],["75630","the"],["75750","device."],["76095",""],["76440",""],["76800","For"],["77160","there"],["77400","to"],["77520","be"],["77730","communication"],["78570","between"],["78990","the"],["79080","two"],["79290","devices,"],["79680",""],["80070","a"],["80250","common"],["80670","standard"],["80940",""],["81210","is"],["81390","required"],["81675",""],["81960","so"],["82170","that"],["82320","both"],["82590","the"],["82680","controller"],["83370","and"],["83730","peripheral"],["84540","understand"],["85230","each"],["85440","other."],["85830",""],["86220","Communications"],["87270","are"],["87420","made"],["87750","with"],["87960","transmissions"],["88710","of"],["88860","words"],["89250","in"],["89370","binary"],["89640",""],["89910","notation."],["90375",""],["90840",""],["91200","These"],["91530","communication"],["92370","bits"],["92700","of"],["92850","1s"],["93210","and"],["93330","0s"],["93615",""],["93900","are"],["94110","often"],["94590","organized"],["95310","in"],["95430","groups"],["95790","of"],["95940","eight,"],["96120","known"],["96390","as"],["96540","a"],["96600","byte."],["96855",""],["97110",""],["97530","For"],["97800","convenience,"],["98550","bytes"],["98910","can"],["99060","be"],["99210","organized"],["99900","into"],["100140","two"],["100380","digital"],["100650",""],["100920","hexadecimal"],["101700","numbers."],["102075",""],["102450",""],["102930","Often,"],["103185",""],["103440","several"],["103830","bytes"],["104190","are"],["104340","used"],["104625",""],["104910","to"],["105090","send"],["105360","data"],["105690","back"],["105990","and"],["106080","forth"],["106440","between"],["106860","the"],["106980","microcontroller"],["107910","controller"],["108660","and"],["109050","peripheral"],["109740","device."],["110070",""],["110400",""],["110655",""],["110910","Multiple"],["111165",""],["111420","bytes"],["111780","may"],["111990","be"],["112170","used"],["112425",""],["112680","to"],["112860","represent"],["113160",""],["113460","the"],["113610","output"],["114030","data"],["114360","for"],["114570","ADCs,"],["115065",""],["115560","output"],["115815",""],["116070","voltages"],["116370",""],["116670","for"],["116820","DACs,"],["117120",""],["117420","or"],["117720","to"],["117870","send"],["118230","commands"],["118515",""],["118800","and"],["119130","configurations"],["120150","to"],["120300","the"],["120390","data"],["120720","converter."],["121410",""],["121830","Digital"],["122310","communications"],["123300","can"],["123480","take"],["123780","many"],["124050","forms,"],["124350",""],["124650","but"],["124860","there"],["125010","are"],["125160","two"],["125490","primary"],["125790",""],["126090","structures"],["126750","that"],["126930","are"],["127050","often"],["127305",""],["127560","used."],["127890",""],["128220",""],["128550","First,"],["128895",""],["129240","the"],["129389","communications"],["130320","can"],["130500","be"],["130620","parallel"],["131010",""],["131400","where"],["131640","one"],["131910","line"],["132210","is"],["132360","used"],["132750","for"],["132900","each"],["133200","bit"],["133380","of"],["133500","data."],["133880",""],["134260","For"],["134580","example,"],["134960",""],["135340","a"],["135390","single"],["135750","byte"],["136020","is"],["136170","transmitted"],["136860","over"],["137160","eight"],["137460","parallel"],["137760",""],["138060","digital"],["138510","lines"],["138900","at"],["139020","once."],["139305",""],["139590",""],["140070","Second,"],["140430",""],["140790","the"],["140940","communications"],["141870","can"],["142020","be"],["142170","serial"],["142500",""],["142830","where"],["143070","all"],["143280","the"],["143400","data"],["143700","bits"],["144000","are"],["144120","on"],["144300","a"],["144360","single"],["144780","digital"],["145260","line."],["145545",""],["145830",""],["146190","In"],["146520","a"],["146610","serial"],["146865",""],["147120","communication,"],["148170","bits"],["148500","are"],["148620","sent"],["148890","serially,"],["149310",""],["149730","one"],["150090","after"],["150450","another."],["150735",""],["151020",""],["151440","Serial"],["151725",""],["152010","communications"],["152910","are"],["153000","more"],["153240","widely"],["153690","used"],["154080","in"],["154200","modern"],["154590","devices,"],["154950",""],["155310","reducing"],["155625",""],["155940","the"],["156030","number"],["156390","of"],["156540","communication"],["157380","lines"],["157710","between"],["158100","the"],["158190","controller"],["158880","and"],["159090","to"],["159210","the"],["159330","peripheral"],["159960","device."],["160260",""],["160560",""],["160950","The"],["161070","figures"],["161520","here"],["161790","show"],["162090","the"],["162210","data"],["162540","going"],["162840","from"],["163140","the"],["163260","controller"],["163920","to"],["164220","the"],["164340","peripheral,"],["165150","but"],["165360","separate"],["165750","lines"],["166110","are"],["166230","required"],["166530",""],["166830","for"],["167010","transmitting"],["167670","data"],["168000","from"],["168270","the"],["168390","peripheral"],["169140","back"],["169440","to"],["169560","the"],["169680","controller."],["170670","For"],["171030","precision"],["171300",""],["171570","data"],["171870","converters,"],["172740","most"],["173190","use"],["173460","forms"],["173880","of"],["174000","serial"],["174450","communication."],["175620",""],["175980","Most"],["176460","TI"],["176910","devices"],["177225",""],["177540","use"],["177780","one"],["178020","of"],["178170","two"],["178410","different"],["178830","serial"],["179085",""],["179340","interface"],["179970","standards,"],["180750",""],["180990","using"],["181440","either"],["181800","4-wire"],["182160",""],["182520","serial"],["182775",""],["183030","peripheral"],["183660","interface"],["184500","or"],["184750","a"],["184830","2-wire"],["185100",""],["185520","I2C."],["185710",""],["185970",""],["186255",""],["186540",""],["186960","This"],["187230","presentation"],["188040","discusses"],["188325",""],["188610","SPI"],["189090","in"],["189240","its"],["189420","implementation."],["190680","I2C"],["191040",""],["191490","is"],["191670","discussed"],["191985",""],["192300","in"],["192450","a"],["192510","different"],["192900","presentation."],["193950",""],["194205",""],["194460","The"],["194610","lines"],["194865",""],["195120","between"],["195570","the"],["195690","controller"],["196350","and"],["196710","the"],["196830","peripheral"],["197520","device"],["197820",""],["198120","are"],["198330","driven"],["198720","to"],["198900","one"],["199140","of"],["199320","two"],["199620","voltage"],["199875",""],["200130","levels."],["200460",""],["200790",""],["201000","If"],["201300","the"],["201390","voltage"],["201645",""],["201900","is"],["202050","near"],["202290","0,"],["202605",""],["202920","then"],["203160","the"],["203250","line"],["203640","is"],["203820","decoded"],["204090",""],["204360","as"],["204570","a"],["204630","digital"],["204885",""],["205140","0."],["205455",""],["205770",""],["205980","If"],["206280","the"],["206370","voltage"],["206625",""],["206880","is"],["207120","near"],["207390","the"],["207510","digital"],["207990","supply,"],["208350",""],["208710","then"],["208920","the"],["209010","line"],["209400","is"],["209550","decoded"],["209820",""],["210090","as"],["210270","a"],["210330","digital"],["210585",""],["210840","1."],["211135",""],["211430",""],["211830","Note"],["212190","that"],["212340","both"],["212580","the"],["212700","controller"],["213300","and"],["213660","the"],["213810","peripheral"],["214650","need"],["214920","to"],["215160","agree"],["215520","what"],["215760","these"],["216030","levels"],["216420","are"],["216750","so"],["217020","that"],["217170","the"],["217290","communication"],["218190","is"],["218370","decoded"],["218640",""],["218910","correctly."],["219810",""],["220110","Digital"],["220380",""],["220650","outputs"],["220935",""],["221220","must"],["221550","be"],["221670","driven"],["222030","high"],["222270","enough"],["222600","to"],["222750","be"],["222930","decoded"],["223230",""],["223530","as"],["223740","a"],["223770","digital"],["224220","1"],["224475",""],["224730","and"],["225180","driven"],["225570","low"],["225810","enough"],["226170","to"],["226290","be"],["226470","decoded"],["226770",""],["227070","as"],["227250","a"],["227310","digital"],["227565",""],["227820","0."],["228120",""],["228420",""],["228750","The"],["228900","data"],["229230","sheet"],["229500","defines"],["229800",""],["230100","the"],["230220","minimum"],["230700","output"],["231150","voltage"],["231405",""],["231660","high"],["231900","level"],["232380","and"],["232740","the"],["232860","maximum"],["233160",""],["233460","output"],["233910","voltage"],["234360","for"],["234610","a"],["234690","low"],["234960","level"],["235350","for"],["235620","a"],["235680","digital"],["235950",""],["236220","output."],["236540",""],["236860",""],["237240","Additionally,"],["238200","the"],["238350","data"],["238650","sheet"],["238950","defines"],["239205",""],["239460","the"],["239580","minimum"],["239835",""],["240090","input"],["240510","voltage"],["240795",""],["241080","that"],["241260","defines"],["241530",""],["241800","a"],["241860","high"],["242100","level"],["242550","and"],["242910","the"],["243030","maximum"],["243315",""],["243600","input"],["244020","voltage"],["244290",""],["244560","that"],["244740","defines"],["245010",""],["245280","a"],["245340","low"],["245610","level."],["245865",""],["246120",""],["246600","Their"],["246780","communication"],["247650","standards"],["247950",""],["248250","define"],["248730","these"],["249030","levels"],["249285",""],["249540","based"],["249930","on"],["250110","the"],["250170","voltage"],["250425",""],["250680","of"],["250830","the"],["250950","digital"],["251205",""],["251460","supply."],["251820",""],["252180",""],["252490","If"],["252750","the"],["252870","controller"],["253500","and"],["253830","peripheral"],["254520","digital"],["254775",""],["255030","supplies"],["255315",""],["255600","do"],["255750","not"],["255960","match,"],["256215",""],["256470",""],["256779","then"],["256920","there"],["257100","may"],["257339","be"],["257490","problems"],["257759",""],["258029","with"],["258269","communications."],["259589",""],["259860","A"],["260070","voltage"],["260550","level"],["260850","translation"],["261570","device"],["262019","may"],["262230","be"],["262410","required"],["262770",""],["263130","to"],["263280","bridge"],["263670","the"],["263790","communications"],["264810","from"],["265020","one"],["265290","supply"],["265770","level"],["266100","to"],["266310","another."],["266580",""],["266850",""],["267120",""],["267390","Communications"],["268440","also"],["268920","require"],["269295",""],["269670","a"],["269850","common"],["270300","timing"],["270780","between"],["271170","the"],["271290","controller"],["271980","and"],["272290","to"],["272340","the"],["272490","peripheral"],["273180","device."],["273510",""],["273840",""],["274140","The"],["274260","two"],["274500","devices"],["274860",""],["275220","must"],["275550","agree"],["275880","on"],["276060","the"],["276150","timing,"],["276555",""],["276960","knowing"],["277380","when"],["277560","the"],["277650","voltage"],["278130","level"],["278460","should"],["278700","be"],["278850","read"],["279120","by"],["279330","the"],["279450","peripheral"],["280080","device"],["280365",""],["280650","to"],["280800","define"],["281055",""],["281310","when"],["281550","the"],["281640","bit"],["281850","transmission"],["282570","occurs."],["282930",""],["283290",""],["283680","Often,"],["284040",""],["284400","a"],["284550","serial"],["284805",""],["285060","clock"],["285420","from"],["285630","the"],["285720","controller"],["286440","is"],["286740","used"],["287160","to"],["287340","define"],["287820","the"],["287910","timing"],["288390","of"],["288570","communication."],["289770",""],["290220","Reading"],["290670","the"],["290760","bit"],["291000","may"],["291240","occur"],["291690","on"],["291900","the"],["291990","rising"],["292290",""],["292590","or"],["292860","falling"],["293340","edges"],["293730","of"],["293880","the"],["294000","serial"],["294480","clock."],["294750",""],["295020",""],["295410","In"],["295680","this"],["295950","example,"],["296375",""],["296800","the"],["296820","data"],["297180","is"],["297420","read"],["297690","on"],["297840","the"],["297930","falling"],["298410","edge"],["298710","of"],["298830","the"],["298920","serial"],["299175",""],["299430","clock."],["299820",""],["300075",""],["300330","Timing"],["300600",""],["300870","is"],["301020","important"],["301305",""],["301590","to"],["301800","the"],["301920","communications"],["303030","and"],["303360","is"],["303570","described"],["303855",""],["304140","in"],["304290","a"],["304350","different"],["304740","video."],["305055",""],["305370",""],["305655",""],["305940","The"],["306120","most"],["306510","common"],["306990","serial"],["307260",""],["307530","interface"],["308280","used"],["308670","in"],["308790","precision"],["309045",""],["309300","data"],["309630","converters"],["310410","is"],["310620","a"],["310680","standard"],["310950",""],["311220","known"],["311550","as"],["311700","serial"],["311955",""],["312210","peripheral"],["312870","interface,"],["313650","abbreviated"],["314550","as"],["314760","SPI."],["315080",""],["315400",""],["315780","There"],["316020","are"],["316200","two"],["316440","control"],["316890","lines"],["317280","for"],["317460","SPI."],["317790",""],["318120","The"],["318300","controller,"],["319020","usually"],["319305",""],["319590","a"],["319680","microcontroller"],["320640","or"],["320820","DSP,"],["321240",""],["321660","controls"],["321960",""],["322260","the"],["322380","peripheral"],["323070","select"],["323400",""],["323730","and"],["324210","the"],["324330","serial"],["324780","clock"],["325035",""],["325290","used"],["325680","for"],["325830","data"],["326130","synchronization."],["327420",""],["327780","A"],["327990","SPI"],["328350","bus"],["328680","can"],["328890","control"],["329370","multiple"],["329850","peripherals,"],["330660","but"],["330870","there"],["331020","can"],["331230","only"],["331590","be"],["331740","one"],["332040","controller."],["332850",""],["333270","Each"],["333600","peripheral"],["334260","requires"],["334590",""],["334920","its"],["335100","own"],["335340","peripheral"],["336030","select"],["336480","line"],["336780","from"],["337020","the"],["337140","controller."],["337990",""],["338430","Additionally,"],["339360","there"],["339600","are"],["339750","two"],["340050","data"],["340380","lines."],["340680",""],["340980",""],["341280","One"],["341580","line"],["341910","sends"],["342270","data"],["342570","from"],["342780","the"],["342870","controller"],["343440","to"],["343650","the"],["343830","peripheral"],["344610","and"],["344850","another"],["345270","sends"],["345600","data"],["345930","from"],["346170","the"],["346260","peripheral"],["347010","to"],["347190","the"],["347310","controller."],["348150",""],["348510","The"],["348690","data"],["349020","transmission"],["349710","may"],["349920","be"],["350100","full"],["350370","duplex,"],["350745",""],["351120","meaning"],["351510","that"],["351660","data"],["352020","can"],["352170","be"],["352320","transmitted"],["353010","in"],["353130","both"],["353460","directions"],["354150","at"],["354300","the"],["354390","same"],["354750","time,"],["355050",""],["355350",""],["355680","using"],["356130","the"],["356220","same"],["356580","SCLK"],["356790",""],["357120","pulses"],["357375",""],["357630","for"],["357780","clocking"],["358035",""],["358290","data."],["358565",""],["358840",""],["359220","The"],["359400","next"],["359730","slides"],["360000",""],["360270","describe"],["360540",""],["360810","the"],["360900","four"],["361200","SPI"],["361580","lines."],["361900",""],["362220",""],["362670","SS"],["363030",""],["363390","is"],["363600","the"],["363720","peripheral"],["364420","select."],["364730",""],["365040",""],["365250","This"],["365580","line"],["365940","is"],["366090","used"],["366345",""],["366600","to"],["366750","select"],["367230","the"],["367350","peripheral"],["367950","device"],["368205",""],["368460","for"],["368700","communication."],["369900",""],["370390","If"],["370650","there"],["370860","are"],["371010","multiple"],["371265",""],["371520","devices"],["371820",""],["372120","on"],["372270","the"],["372360","SPI"],["372720","bus,"],["372995",""],["373270","each"],["373620","device"],["374100","has"],["374310","its"],["374490","own"],["374730","peripheral"],["375420","select."],["375720",""],["376020",""],["376290","Peripheral"],["376990","select"],["377460","is"],["377610","often"],["378090","used"],["378510","as"],["378670","active"],["379050","low,"],["379470","indicated"],["380190","by"],["380430","an"],["380580","overbar."],["380880",""],["381150",""],["381420",""],["381780","When"],["382110","the"],["382200","device"],["382650","is"],["382800","selected,"],["383160",""],["383520","peripheral"],["384210","select"],["384660","goes"],["384945","low"],["385230","to"],["385410","activate"],["385980","communication."],["387090",""],["387450","When"],["387720","the"],["387810","device"],["388260","is"],["388410","not"],["388680","selected,"],["389040",""],["389400","the"],["389550","peripheral"],["390190","select"],["390690","is"],["390810","set"],["391110","high."],["391365",""],["391620",""],["392040","Peripheral"],["392710","select"],["393180","may"],["393390","also"],["393750","be"],["393930","labeled"],["394350","as"],["394650","SSEL,"],["395020",""],["395390",""],["395760","CS,"],["396150",""],["396540","CS"],["396930",""],["397180","bar,"],["397680","CE,"],["398130",""],["398580","nSS,"],["398940",""],["399345","or"],["399750","SS#."],["400230",""],["400545",""],["400860",""],["401190","In"],["401490","many"],["401760","precision"],["402045",""],["402330","ADCs"],["402660",""],["402990","from"],["403290","TI,"],["403605",""],["403920",""],["404160","this"],["404400","chip"],["404670","select"],["405090","line"],["405360","is"],["405510","commonly"],["405810",""],["406110","labeled"],["406500","as"],["406680","CS"],["407175","bar,"],["407670","used"],["408090","as"],["408270","active"],["408690","low."],["409140",""],["409500","In"],["409740","many"],["410070","TI"],["410460","precision"],["410715",""],["410970","DACs,"],["411285",""],["411600","this"],["411870","line"],["412200","is"],["412380","commonly"],["412665",""],["412950","labeled"],["413370","as"],["413520","SYNC"],["413820","bar,"],["414180",""],["414540","also"],["414900","active"],["415380","low."],["415830",""],["416175",""],["416520","SCLK"],["416910",""],["417300","is"],["417540","the"],["417630","serial"],["417915",""],["418200","clock."],["418485",""],["418770",""],["418980","As"],["419400","mentioned"],["419655",""],["419910","previously,"],["420900","SCLK"],["421170",""],["421590","is"],["421740","used"],["422070","by"],["422280","the"],["422400","controller"],["422970","to"],["423120","synchronize"],["423870","the"],["423990","data"],["424320","sent"],["424680","between"],["425100","the"],["425220","controller"],["425940","and"],["426300","the"],["426450","peripheral"],["427080","device."],["427380",""],["427680",""],["428040","The"],["428250","SCLK"],["428490",""],["428850","originates"],["429510","from"],["429720","the"],["429840","controller"],["430500","and"],["430740","is"],["430860","sent"],["431100","to"],["431310","all"],["431520","peripheral"],["432180","devices."],["432630",""],["433080",""],["433500","This"],["433770","serial"],["434220","clock"],["434610","may"],["434790","not"],["435060","always"],["435480","be"],["435660","in"],["435810","operation"],["436680","and"],["437100","may"],["437310","be"],["437520","idle"],["437910","as"],["438150","a"],["438240","high"],["438540","or"],["438660","low"],["438960","signal."],["439275",""],["439590",""],["440040","Data"],["440400","is"],["440610","clocked"],["440970","into"],["441120",""],["441270","the"],["441390","controller"],["442020","or"],["442260","peripheral"],["443110","at"],["443370","either"],["443700","the"],["443820","rising"],["444075",""],["444330","edge"],["444690","or"],["444930","falling"],["445380","edge"],["445620","of"],["445740","the"],["445830","serial"],["446085",""],["446340","clock."],["446820",""],["447180","The"],["447390","SCLK"],["447660",""],["448020","line"],["448350","may"],["448560","also"],["448920","be"],["449100","labeled"],["449540","as"],["449780","SCK."],["450240",""],["450690",""],["451020",""],["451350","MOSI"],["451725",""],["452100","is"],["452400","the"],["452550","controller"],["453180","out,"],["453600","peripheral"],["454320","in."],["454620",""],["454920",""],["455160","This"],["455490","line"],["455820","is"],["456000","used"],["456480","to"],["456630","send"],["456870","data"],["457200","from"],["457440","the"],["457530","controller"],["458100","to"],["458280","the"],["458400","peripheral"],["459060","device."],["459375",""],["459690",""],["459900","The"],["460170","peripheral"],["460800","device"],["461280","reads"],["461610","the"],["461700","MOSI"],["462150","line"],["462405",""],["462660","based"],["463080","on"],["463260","synchronization"],["464190","from"],["464460","the"],["464610","SCLK."],["464820",""],["465090",""],["465360",""],["465630","Again,"],["465975",""],["466320","this"],["466590","line"],["466920","may"],["467100","have"],["467340","different"],["467700","names"],["468090","depending"],["468570","on"],["468750","the"],["468840","device"],["469320","manufacturer."],["470430",""],["470820","On"],["471130","the"],["471240","peripheral"],["471810","device,"],["472145",""],["472480","it"],["472590","may"],["472800","be"],["472980","known"],["473310","as"],["473490","SIMO,"],["473835",""],["474180","SDI,"],["474520",""],["474860",""],["475200","DI,"],["475590",""],["475980","DN,"],["476355",""],["476730","or"],["477060","SI."],["477420",""],["477780",""],["478110","This"],["478440","line"],["478770","is"],["478920","connected"],["479175",""],["479430","to"],["479610","the"],["479730","controller"],["480300","device"],["480600",""],["480900","on"],["481140","some"],["481440","serial"],["481755",""],["482070","outline"],["482385",""],["482700","labeled"],["483120","as"],["483490","SDO,"],["483965",""],["484440","DO,"],["484830",""],["485160","or"],["485430","DOUT."],["485700",""],["486180",""],["486540","In"],["486780","precision"],["487065",""],["487350","data"],["487650","converters,"],["488400","if"],["488730","there"],["488940","are"],["489060","registers"],["489405",""],["489750","that"],["489930","require"],["490200",""],["490470","configuration,"],["491610","the"],["491820","configuration"],["492720","data"],["493050","are"],["493260","sent"],["493650","on"],["493830","this"],["494040","line."],["494325",""],["494610",""],["494970","If"],["495270","the"],["495420","device"],["495870","is"],["496020","not"],["496290","active,"],["496575",""],["496860","as"],["497130","the"],["497250","controller"],["497820","has"],["498030","not"],["498240","selected"],["498540",""],["498840","the"],["498990","device"],["499440","to"],["499560","be"],["499740","active"],["500220","with"],["500460","peripheral"],["501100","select,"],["501395",""],["501690",""],["502080","this"],["502380","line"],["502680","is"],["502860","deactivated,"],["503790","and"],["504030","the"],["504120","peripheral"],["504720","does"],["504960","not"],["505170","receive"],["505620","data"],["505980","on"],["506220","MOSI."],["506550",""],["506880",""],["507210","In"],["507480","many"],["507830","precision"],["508090",""],["508350","data"],["508680","converters,"],["509550","TI"],["510030","commonly"],["510315",""],["510600","labels"],["511050","this"],["511380","digital"],["511650",""],["511920","input"],["512400","as"],["512730","DN."],["513000",""],["513480",""],["513960","MISO"],["514379",""],["514799","is"],["515070","controller"],["515730","in,"],["516150","peripheral"],["516900","out."],["517350",""],["517710","This"],["518010","line"],["518340","is"],["518520","used"],["519000","to"],["519150","send"],["519419","data"],["519750","from"],["520020","the"],["520110","peripheral"],["520770","device"],["521085",""],["521400","out"],["521669","to"],["521820","the"],["521940","controller."],["522750",""],["523049","If"],["523380","the"],["523530","controller"],["524100","has"],["524340","not"],["524580","selected"],["524865",""],["525150","the"],["525270","device"],["525690","to"],["525810","be"],["525990","active"],["526470","with"],["526710","peripheral"],["527350","select,"],["527630",""],["527910",""],["528180","this"],["528450","line"],["528750","becomes"],["529170","high"],["529410","impedance,"],["530130","or"],["530370","Hi-Z,"],["530670",""],["530955",""],["531240","allowing"],["531555",""],["531870","for"],["532080","a"],["532170","system"],["532590","with"],["532770","multiple"],["533250","devices"],["533580",""],["533910","to"],["534030","share"],["534390","this"],["534630","line."],["534915",""],["535200",""],["535620","The"],["535800","peripheral"],["536460","device"],["536880","sends"],["537240","data"],["537570","out"],["537900","on"],["538050","the"],["538140","MISO"],["538620","line"],["539100","and"],["539310","is"],["539430","synchronized"],["540210","with"],["540360","the"],["540510","SCLK."],["540900",""],["541290",""],["541680","On"],["541950","the"],["542100","peripheral"],["542760","device,"],["543140",""],["543520","it"],["543630","may"],["543870","be"],["544020","known"],["544350","as"],["544770","SOMI,"],["545160",""],["545530","SDO,"],["545990",""],["546450","DO,"],["546825",""],["547200",""],["547410","DOUT,"],["547755",""],["548100","or"],["548370","SO."],["548730",""],["549090",""],["549510","This"],["549810","line"],["550110","is"],["550260","connected"],["550710","to"],["550860","the"],["551010","controller"],["551550","device"],["551850",""],["552150","on"],["552360","some"],["552630","serial"],["552900",""],["553170","outline"],["553455",""],["553740","labeled"],["554160","as"],["554550","SDI,"],["555015",""],["555480","DI,"],["555960","or"],["556440","DN."],["556830",""],["557220",""],["557550","In"],["557790","many"],["558090","precision"],["558360",""],["558630","data"],["558900","converters,"],["559650","TI"],["560130","commonly"],["560415",""],["560700","labels"],["561180","this"],["561420","digital"],["561675",""],["561930","output"],["562185",""],["562440","as"],["562710","DOUT."],["562980",""],["563400",""],["563790","As"],["564150","previously"],["564930","mentioned,"],["565650","data"],["566040","from"],["566280","the"],["566370","controller"],["567060","and"],["567450","peripheral"],["568260","may"],["568530","be"],["568680","read"],["568950","on"],["569160","either"],["569460","the"],["569610","rising"],["569880",""],["570150","or"],["570450","falling"],["570900","edge"],["571140","of"],["571260","SCLK."],["571620",""],["571980",""],["572310","Additionally,"],["573270","the"],["573420","clock"],["573780","polarity"],["574410","is"],["574560","important"],["574860",""],["575160","in"],["575280","defining"],["575565",""],["575850","the"],["575970","leading"],["576420","and"],["576750","trailing"],["577005",""],["577260","edges"],["577740","on"],["577950","which"],["578250","the"],["578340","data"],["578670","is"],["578880","clocked"],["579270","in"],["579600","and"],["579900","out"],["580170","of"],["580440","the"],["580590","device."],["580890",""],["581190",""],["581495",""],["581800","This"],["582000","enables"],["582450","several"],["582870","modes"],["583230","of"],["583320","SPI"],["583650","communication."],["584760",""],["585120","There"],["585360","are"],["585540","two"],["585780","parameters"],["586620","used"],["586980","to"],["587130","determine"],["587640","modes"],["588000","of"],["588150","operation."],["589110",""],["589600","The"],["589680","first"],["590040","parameter,"],["590790","CPOL,"],["591180",""],["591435",""],["591690","determines"],["592320","the"],["592440","clock"],["592770","polarity"],["593280","for"],["593490","the"],["593700","serial"],["594060","clock."],["594420",""],["594780","When"],["595170","CPOL"],["595470",""],["595800","equals"],["596190","0,"],["596505",""],["596820","then"],["597120","the"],["597210","clock"],["597630","idles"],["598050","low."],["598365",""],["598680","The"],["598970","leading"],["599300","edge"],["599540","is"],["599690","a"],["599780","rising"],["600035",""],["600290","edge,"],["600710","and"],["601040","the"],["601160","trailing"],["601430",""],["601700","edge"],["602060","is"],["602270","a"],["602330","falling"],["602585",""],["602840","edge."],["603320",""],["603620","When"],["603950","CPOL"],["604220",""],["604580","is"],["604760","equal"],["605060","to"],["605210","1,"],["605480",""],["605750","the"],["605900","clock"],["606290","idles"],["606680","high."],["606950",""],["607220",""],["607680","The"],["607760","leading"],["608180","edge"],["608450","is"],["608580","a"],["608660","falling"],["609140","edge,"],["609500","and"],["609710","the"],["609800","trailing"],["610055",""],["610310","edge"],["610640","is"],["610830","a"],["610910","rising"],["611390","edge."],["611860",""],["612135",""],["612410","The"],["612590","second"],["613070","parameter,"],["613820","CPHA,"],["614240",""],["614660",""],["615080","determines"],["615830","the"],["615950","clock"],["616280","phase"],["616670","for"],["616850","which"],["617150","the"],["617270","data"],["617660","is"],["617900","acquired."],["618260",""],["618620",""],["618980","For"],["619340","the"],["619460","CPHA"],["619690",""],["620085",""],["620480","equal"],["620840","to"],["620990","0,"],["621335",""],["621680","data"],["622100","is"],["622310","captured"],["622565",""],["622820","on"],["623000","the"],["623090","leading"],["623510","edge"],["623750","of"],["623870","the"],["623960","clock"],["624320","pulse."],["624800",""],["625190","Data"],["625580","is"],["625760","set"],["626030","up"],["626240","on"],["626390","the"],["626480","trailing"],["626735",""],["626990","edge"],["627260","of"],["627410","SCLK"],["627590",""],["627980","for"],["628160","the"],["628250","first"],["628640","bit"],["629030","when"],["629330","SS"],["629810","bar"],["630110","is"],["630290","set"],["630560","low."],["630830",""],["631100",""],["631370","For"],["631730","CPHA"],["632110",""],["632490",""],["632870","equal"],["633260","to"],["633410","1,"],["633860",""],["634160","the"],["634340","data"],["634700","is"],["634910","captured"],["635390","on"],["635540","the"],["635660","trailing"],["636140","edge"],["636380","of"],["636500","SCLK."],["636860",""],["637220",""],["637460","In"],["637730","both"],["638060","clock"],["638420","phase"],["638780","modes,"],["639080",""],["639380","data"],["639800","is"],["639980","set"],["640220","up"],["640430","on"],["640580","the"],["640700","previous"],["641000",""],["641300","clock"],["641660","edge."],["642110",""],["642600",""],["643090",""],["643580","Combinations"],["644570","of"],["644690","CPOL"],["645065",""],["645440","and"],["645770","CPHA"],["646160",""],["646550",""],["646940","allow"],["647390","for"],["647600","four"],["647930","modes"],["648320","of"],["648470","operation"],["649190","of"],["649340","SPI."],["649655",""],["649970",""],["650270","The"],["650450","table"],["650900","in"],["651080","this"],["651230","slide"],["651650","shows"],["651990","SPI"],["652340","mode"],["652640","0"],["653060","through"],["653330","3."],["653810",""],["654200","Each"],["654590","defines"],["654845",""],["655100","a"],["655160","different"],["655520","clock"],["655910","polarity"],["656600","and"],["656990","phase"],["657440","for"],["657620","SPI"],["657950","communication."],["659090",""],["659510","Note"],["659930","that"],["660140","different"],["660470","manufacturers"],["661580","of"],["661700","SPI"],["662060","devices"],["662465",""],["662870","and"],["663260","microcontrollers"],["664460","may"],["664790","have"],["665030","different"],["665390","definitions"],["666170","of"],["666320","SPI"],["666710","mode"],["667100","numbers."],["667430",""],["667760",""],["668090","Consult"],["668360",""],["668630","the"],["668720","data"],["669020","sheets"],["669380","for"],["669530","both"],["669800","the"],["669920","controller"],["670580","and"],["670970","peripherals"],["671810","to"],["671960","determine"],["672530","the"],["672620","clock"],["672950","polarity"],["673640","and"],["674030","phase"],["674450","information."],["675380",""],["675770","SPI"],["676045",""],["676320","can"],["676520","be"],["676700","used"],["676985",""],["677270","to"],["677420","communicate"],["678170","with"],["678350","multiple"],["678605",""],["678860","devices."],["679315",""],["679770",""],["680160","This"],["680360","can"],["680540","be"],["680690","done"],["681020","in"],["681170","two"],["681380","different"],["681740","ways."],["682050",""],["682360",""],["682740","First,"],["683005",""],["683270","because"],["683690","SPI"],["684080","uses"],["684560","peripheral"],["685220","select"],["685680","lines,"],["685950",""],["686220","the"],["686390","controller"],["686960","can"],["687140","communicate"],["687890","with"],["688070","multiple"],["688550","devices."],["689015",""],["689480",""],["689840","Each"],["690230","peripheral"],["690950","has"],["691220","its"],["691400","own"],["691580","peripheral"],["692250","select"],["692530",""],["692810","coming"],["693200","from"],["693410","the"],["693500","controller,"],["694220","while"],["694460","the"],["694580","remaining"],["694865",""],["695150","lines"],["695510","are"],["695600","shared."],["695930",""],["696260",""],["696680","When"],["697010","peripheral"],["697710","select"],["698210","is"],["698300","selected"],["698585",""],["698870","for"],["699050","the"],["699170","device,"],["699470",""],["699770",""],["699990","the"],["700190","remaining"],["700460",""],["700730","SPI"],["701090","lines"],["701450","are"],["701570","active."],["701915",""],["702260",""],["702500","When"],["702770","the"],["702920","peripheral"],["703560","select"],["704000","is"],["704150","not"],["704390","selected,"],["704750",""],["705110","the"],["705260","SPI"],["705620","lines"],["705980","are"],["706160","ignored."],["706520",""],["706880",""],["707240","When"],["707510","not"],["707750","selected,"],["708110",""],["708470","each"],["708830","peripheral"],["709580","MOSI"],["709850",""],["710120","and"],["710450","SCLK"],["710660",""],["710690",""],["711050","line"],["711350","is"],["711500","ignored,"],["711875",""],["712250","and"],["712670","each"],["712910","MISO"],["713255","line"],["713600","becomes"],["714050","Hi-Z"],["714365",""],["714680","so"],["714950","that"],["715100","an"],["715280","active"],["715760","peripheral"],["716480","may"],["716690","drive"],["717110","the"],["717200","MISO"],["717410",""],["717650","without"],["718070","contention"],["718760","from"],["719030","other"],["719360","peripherals"],["720110","trying"],["720530","to"],["720650","drive"],["721040","the"],["721160","same"],["721550","line."],["721805",""],["722060",""],["722360",""],["722660","For"],["722990","some"],["723320","systems,"],["723775",""],["724230","a"],["724280","single"],["724760","SPI"],["725150","drives"],["725405",""],["725660","one"],["725900","peripheral"],["726770","while"],["727070","other"],["727430","peripherals"],["728240","are"],["728360","daisy-chained"],["729230","together."],["729575",""],["729920",""],["730250","In"],["730550","a"],["730610","daisy-chained"],["731450","system,"],["731765","SCLKs"],["732080",""],["732455",""],["732830","and"],["733190","peripheral"],["733880","selects"],["734210",""],["734540","may"],["734840","be"],["734990","shared"],["735410","by"],["735620","all"],["735860","peripherals."],["736820",""],["737150","However,"],["737480",""],["737810","the"],["737960","controller"],["738500","connects"],["738950","to"],["739100","a"],["739190","single"],["739610","MOSI"],["739910",""],["740210","of"],["740450","the"],["740570","first"],["740960","peripheral."],["741800",""],["742070","The"],["742250","MISO"],["742520",""],["742790","of"],["742970","the"],["743060","first"],["743510","peripheral"],["744290","connects"],["744545",""],["744800","to"],["744950","the"],["745070","MOSI"],["745400",""],["745550","of"],["745760","the"],["745850","next"],["746240","peripheral."],["747110",""],["747500","This"],["747770","chains"],["748190","all"],["748430","of"],["748580","the"],["748700","peripherals"],["749510","together"],["749855",""],["750200","from"],["750500","one"],["750740","MISO"],["750950",""],["751220","to"],["751400","the"],["751490","next"],["751850","MOSI."],["752165",""],["752480",""],["752900","For"],["753140","the"],["753260","last"],["753650","peripheral"],["754310","device,"],["754625",""],["754940","the"],["755090","MISO"],["755570","connects"],["755990","to"],["756140","the"],["756290","controller."],["757070",""],["757430","All"],["757760","data"],["758120","from"],["758360","the"],["758450","devices"],["758750",""],["759050","are"],["759170","passed"],["759620","through"],["759830","the"],["759980","chain"],["760430","and"],["760790","collected"],["761075",""],["761360","at"],["761510","the"],["761660","end"],["762050","from"],["762350","the"],["762440","final"],["762860","peripheral."],["763700",""],["764000","Not"],["764360","all"],["764600","devices"],["764930",""],["765260","are"],["765440","able"],["765890","to"],["766040","be"],["766250","controlled"],["766970","and"],["767300","read"],["767570","through"],["767870","a"],["767930","daisy-chained"],["768800","SPI"],["769220","connection."],["770090",""],["770420","Devices"],["770765",""],["771110","must"],["771440","be"],["771650","specifically"],["772430","designed"],["772715",""],["773000","for"],["773330","this"],["773570","communication."],["774620",""],["775040","Here"],["775430","is"],["775610","an"],["775730","example"],["776030",""],["776330","of"],["776480","SPI"],["776900","data"],["777260","communication."],["778450",""],["778850","This"],["779120","comes"],["779450","from"],["779660","the"],["779750","communication"],["780650","of"],["780800","the"],["780980","ADS1118"],["781740",""],["782120",""],["782390",""],["782660","precision"],["782975",""],["783290","ADC."],["783680",""],["784070",""],["784460","The"],["784670","ADS1118"],["785690",""],["785975",""],["786260","is"],["786410","a"],["786500","16-bit"],["786770",""],["787040",""],["787310","ADC"],["787715",""],["788120","that"],["788360","uses"],["788780","SPI"],["789200","mode"],["789500","1"],["789980","with"],["790250","CPOL"],["790550",""],["790850","equal"],["791180","to"],["791330","0"],["791615",""],["791900","and"],["792230","CPHA"],["792570",""],["792910",""],["793250","equal"],["793610","to"],["793760","1."],["794060",""],["794360",""],["794840","Here,"],["795110",""],["795380","the"],["795770","SCLK"],["796160","idles"],["796520","low,"],["796970","and"],["797330","the"],["797450","data"],["797780","is"],["797990","clocked"],["798380","in"],["798710","and"],["799040","out"],["799280","of"],["799490","the"],["799610","device"],["799895",""],["800180","on"],["800390","the"],["800450","trailing"],["800720",""],["800990","edge"],["801290","of"],["801460","SCLK."],["801795",""],["802130",""],["802460","In"],["802700","the"],["802850","16-bit"],["803330",""],["803570","data"],["803900","transmission"],["804620","cycle,"],["804920",""],["805220",""],["805460","two"],["805730","bytes"],["806090","of"],["806210","data"],["806540","are"],["806720","clocked"],["807140","into"],["807530","a"],["807620","configuration"],["808610","register."],["809015",""],["809420",""],["809780","At"],["810050","the"],["810140","same"],["810500","time,"],["810980","16"],["811295",""],["811610","bits"],["811880","of"],["812060","ADC"],["812360",""],["812660","data"],["813020","is"],["813230","clocked"],["813650","out"],["813800","of"],["813950","the"],["814070","device."],["814400",""],["814730",""],["815180","The"],["815390","ADC"],["815705",""],["816020","has"],["816260","a"],["816350","16-bit"],["816650",""],["816950",""],["817160","configuration"],["818090","register"],["818525",""],["818960","with"],["819230","settings"],["819710","showing"],["820130","in"],["820280","the"],["820370","table."],["820700",""],["821030",""],["821360","These"],["821690","configuration"],["822620","register"],["822875",""],["823130","values"],["823400",""],["823670","program"],["823940",""],["824210","the"],["824300","device"],["824570",""],["824840","to"],["824990","the"],["825110","settings"],["825410",""],["825710","shown"],["825965","in"],["826220","the"],["826310","description"],["826940","common."],["827225",""],["827510",""],["827930","For"],["828320","this"],["828560","example,"],["828970",""],["829380","the"],["829430","setting"],["829820","we"],["829970","want"],["830210","to"],["830360","write"],["830630","to"],["830810","the"],["830930","device"],["831230",""],["831530","is"],["831770","81C3"],["831990",""],["832326",""],["832662",""],["833000","and"],["833240","hexadecimal."],["834140",""],["834590",""],["835040",""],["835490","Continuing"],["836300","with"],["836480","the"],["836660","example,"],["837130",""],["837600","this"],["837770","is"],["837950","the"],["838100","16-bit"],["838385",""],["838670",""],["838910","data"],["839240","transmission"],["839930","cycle"],["840410","for"],["840680","the"],["840860","ADS1118"],["841880",""],["842195",""],["842510","showing"],["842765",""],["843020","the"],["843110","SPI"],["843470","lines."],["843785",""],["844100",""],["844400","Again,"],["844715",""],["845030","the"],["845240",""],["845450","SCLK"],["845840","idles"],["846230","low,"],["846650","and"],["846890","data"],["847250","is"],["847460","transmitted"],["848150","at"],["848300","the"],["848390","falling"],["848870","edge"],["849140","of"],["849260","SCLK."],["849470",""],["849725",""],["849980",""],["850340","The"],["850490","write"],["850790","to"],["850970","the"],["851060","device"],["851540","is"],["851720","done"],["851960","on"],["852110","the"],["852200","MOSI,"],["852515",""],["852830","or"],["853070","on"],["853250","this"],["853460","device,"],["853730",""],["854000","the"],["854150","pin"],["854510","is"],["854660","labeled"],["855110","as"],["855410","DN."],["855800",""],["856190",""],["856520","The"],["856700","configuration"],["857630","register"],["857960",""],["858290","is"],["858440","set"],["858710","to"],["858860","81C3"],["859130",""],["859460",""],["859730",""],["860210","and"],["860450","hexadecimal."],["861380",""],["861740","At"],["862040","the"],["862130","same"],["862490","time,"],["862760",""],["863030","the"],["863240","ADC"],["863525",""],["863810","data"],["864200","is"],["864440","clocked"],["864830","out"],["864980","of"],["865100","the"],["865280","ADS1118."],["866300",""],["866660",""],["867020",""],["867350","Here,"],["867620",""],["867890","a"],["868040","random"],["868460","output"],["868910","data"],["869210","word"],["869480","is"],["869630","clocked"],["870020","out"],["870170","of"],["870290","the"],["870380","device."],["870710",""],["871040",""],["871520","Looking"],["871940","at"],["872090","the"],["872180","DOUT"],["872660","line,"],["872915",""],["873170","the"],["873260","binary"],["873575",""],["873890","output"],["874370","is"],["874520","read"],["874880","as"],["875150","E476"],["875750",""],["876140",""],["876395",""],["876650","and"],["876890","hexadecimal."],["877820",""],["878300","That"],["878570","concludes"],["878885",""],["879200","this"],["879470","video."],["879805",""],["880140","Thank"],["880430","you"],["880520","for"],["880700","watching."],["881030",""],["881360",""],["881740","Please"],["882020","try"],["882260","the"],["882380","quiz"],["882740","to"],["882860","check"],["883160","your"],["883400","understanding"],["884150","of"],["884270","this"],["884540","video's"],["885020","content."],["885410",""],["885800",""],["886115",""],["886430","Question"],["886745",""],["887060","one."],["887345",""],["887630",""],["887900","The"],["888050","following"],["888350",""],["888650","binary"],["888965",""],["889280","output"],["889595",""],["889910","is"],["890180","what"],["890420","value"],["890900","in"],["891050","hexadecimal?"],["892070",""],["892535",""],["893000",""],["893465",""],["893930",""],["894395",""],["894860",""],["895325",""],["895790","The"],["895970","correct"],["896225",""],["896480","answer"],["896870","is"],["897080","D,"],["897395",""],["897710","A6."],["898070",""],["898415",""],["898760",""],["899177",""],["899594",""],["900011",""],["900430","Question"],["900760",""],["901090","two."],["901390",""],["901690",""],["901990","The"],["902110","following"],["902395",""],["902680","diagram"],["902995",""],["903310","is"],["903460","CPOL"],["903745",""],["904030","equal"],["904360","to"],["904510","0"],["904795",""],["905080","and"],["905350","CPHA"],["905845",""],["906340","equal"],["906700","to"],["906880","1."],["907150",""],["907420",""],["907870","What"],["908140","hexadecimal"],["908920","byte"],["909250","is"],["909370","sent"],["909670","from"],["909910","the"],["910030","peripheral"],["910660","to"],["910840","the"],["910960","controller"],["911590","in"],["911710","this"],["911950","transaction?"],["912910",""],["913358",""],["913806",""],["914254",""],["914702",""],["915150",""],["915598",""],["916046",""],["916500","The"],["916580","correct"],["917060","answer"],["917450","is"],["917630","B,"],["917885",""],["918140","26."],["918530",""],["918830",""],["919130",""],["919593",""],["920056",""],["920520","Question"],["920880",""],["921240","three."],["921570",""],["921900",""],["922110","The"],["922260","following"],["922545",""],["922830","diagram"],["923145",""],["923460","is"],["923610","CPOL"],["923880",""],["924150","equal"],["924510","to"],["924660","0"],["924930",""],["925200","and"],["925410","CPHA"],["925750",""],["926090",""],["926430","equal"],["926790","to"],["926940","1."],["927440",""],["927720","What"],["928050","hexadecimal"],["928860","byte"],["929220","is"],["929340","sent"],["929640","from"],["929910","the"],["930000","controller"],["930570","to"],["930780","the"],["930900","peripheral"],["931590","in"],["931740","this"],["931950","transaction?"],["932940",""],["933411",""],["933882",""],["934353",""],["934824",""],["935295",""],["935766",""],["936237",""],["936710","The"],["936760","correct"],["937210","answer"],["937600","is"],["937780","D,"],["938035",""],["938290","EC."],["938590",""],["938890",""],["939190",""],["939490",""],["939790",""],["940090",""],["940390",""],["940690",""],["940990",""],["941290",""],["941590",""],["941890",""],["942190",""],["942490",""],["942790",""],["943090",""],["943390",""],["943690",""],["943990",""],["944290",""],["944590",""],["944890",""],["945190",""],["945490",""],["945790",""],["946090",""],["946390",""],["946690",""],["946990",""],["947290",""],["947590",""],["947890",""],["948190",""],["948490",""],["948790",""],["949090",""],["949390",""],["949690",""],["949990",""]],"paragraphs":[0,300,31620,66390,86220,121830,151440,175980,194460,228750,267390,305940,338430,362670,381780,416520,451350,478110,513960,535620,563790,585120,612410,643580,675770,696680,722660,752900,775040,802460,835490,861740,878300,886430,900430,920520],"speakers":{}}