{"words":[["2640","大家好！"],["3270","欢迎观看有关"],["4410","通常称为"],["5550","CAN"],["6690","通信的控制器局域网"],["7770","通信的"],["8850","TI"],["9930","高精度实验室视频。"],["11010","该视频将介绍"],["11640","CAN"],["12270","收发器"],["12900","用于通过"],["14017","CAN"],["15135","总线"],["16252","进行通信的方法，"],["17370","尤其是在"],["19070","汽车应用中。"],["20770","该介绍性"],["22625","视频将包括"],["24480","CAN"],["25750","概述、标准"],["27020","简介、物理层"],["28290","介绍以及对不同"],["29663","CAN"],["31036","协议的论述。"],["32409","这是典型的汽车"],["34314","车身网络示例。"],["36220","汽车中的中央"],["37990","车身控制装置"],["39760","或任何类似的"],["41275","主器件需要"],["42790","与汽车中其他"],["43945","通常远离主器件"],["45100","本身的器件"],["46270","进行通信，"],["47440","以完成各种任务。"],["49680","此处以蓝色"],["50395","显示的"],["51110","CAN"],["51825","总线"],["52540","允许组件在汽车中"],["54565","彼此无缝通信。"],["56590","以黄色显示的"],["57482","LIN"],["58375","总线"],["59267","允许进一步扩展到"],["60160","外围器件。"],["62470","例如，使用该总线"],["63805","网络，空调系统"],["65140","可以与电动座椅"],["66445","系统相连接，以激活"],["67750","座椅加热器，"],["69310","或者控制单元"],["70870","可以在踩下"],["72370","制动踏板时"],["73870","激活制动灯。"],["76530","该总线层次结构设计"],["78720","可以节省线路成本。"],["80910","线路是汽车中"],["82790","最昂贵的部件之一。"],["84670","它很重并且"],["85940","通常手工组装。"],["87210","因此，线路对汽车的"],["89175","整体生产成本具有"],["91140","直接的影响。"],["92700","汽车设计人员使用"],["93825","CAN"],["94950","来"],["96075","最大程度地减少汽车中的"],["97200","线路，从而降低制造"],["99615","成本并提高燃油效率。"],["102030","CAN"],["103453","是当今汽车中"],["104876","使用的主要总线。"],["106300","它使电动座椅、"],["107960","车门模块和"],["109620","空调单元等不同的"],["111265","模块能够相互通信。"],["112910","具有灵活数据"],["113471","速率的"],["114033","CAN"],["114595","或"],["115156","CAN"],["115718","FD"],["116280","是通过该总线进行"],["118380","通信的最常用的方法。"],["120480","CAN"],["121290","和"],["122100","CAN"],["122910","FD"],["123720","实现差分两线制"],["124530","接口。"],["125850","传统"],["126574","CAN"],["127299","的运行速率"],["128024","最高为"],["128749","1"],["129474","兆位/秒，而"],["130199","CAN"],["130992","FD"],["131786","的运行速率"],["132579","最高为"],["133373","5"],["134166","兆位/秒。"],["134960","LIN"],["136786","是以较低数据"],["138613","速率运行的子总线。"],["140440","CAN"],["141746","标准为多点"],["143053","总线应用中的"],["144360","异步串行通信"],["146280","定义了协议和"],["148200","物理层。"],["149790","每个节点由一个"],["150291","MCU"],["150792","中的"],["151294","一个"],["151795","CAN"],["152297","收发器和一个"],["152798","CAN"],["153300","控制器构成。"],["155880","传统"],["156350","CAN"],["156820","通过差分"],["157290","总线以高达"],["157760","1"],["158230","兆位/秒的"],["158700","数据速率进行通信，"],["160320","而具有灵活数据速率的"],["161940","CAN"],["162629","以高达"],["163318","5"],["164007","兆位/秒的"],["164696","数据速率进行通信。"],["165385","CAN"],["166986","专为与双绞线"],["168588","电缆配合使用而设计。"],["170190","网络应采用总线拓扑"],["171525","结构进行布线，从而"],["172860","尽可能限制"],["174840","末梢区域数量。"],["176820","用于"],["177347","CAN"],["177874","和"],["178401","CAN"],["178928","FD"],["179455","的"],["179982","总线的两端应使用与"],["180510","网络阻抗"],["181785","匹配的电阻器"],["183060","正确端接。"],["185040","正确的端接有助于"],["186450","减少等信号完整性问题，"],["187860","例如反射。"],["189480","如果从"],["190590","总线中移除"],["191700","节点，则设计人员在选择"],["193095","放置端接电阻器的位置时"],["194490","必须格外小心。"],["196760","可以通过不同的"],["198275","方法实现端接。"],["199790","标准端接在总线的"],["201500","两端各使用一个"],["203210","端接电阻器。"],["205250","一种替代方法"],["206480","是分裂端接，"],["207710","如右图所示，"],["209495","它可以改善"],["211280","信号完整性和"],["212825","电磁发射特性。"],["214370","它还可以"],["215300","消除总线"],["216230","共模电压"],["217550","电平的波动，"],["218870","同时保留"],["220755","差分波动。"],["222640","采用双绞线"],["223382","布线的"],["224125","CAN"],["224867","总线"],["225610","拓扑通常具有"],["227090","120"],["228570","欧姆的特性阻抗。"],["230050","因此，正确的端接通常"],["231242","需要使用"],["232435","120"],["233627","欧姆的"],["234820","端接电阻器。"],["237520","由于"],["238055","CAN"],["238591","网络将"],["239127","CANH"],["239662","和"],["240198","CANL"],["240734","连接至"],["241270","VCC"],["242300","和接地等"],["243330","电源，因此端接"],["244360","电阻器的"],["245680","额定功率"],["247000","应考虑网络中"],["247800","CAN"],["248600","收发器的"],["249400","短路电流保护。"],["254890","CAN"],["256059","是两线制"],["257229","差分信号。"],["258399","差分电压"],["259349","VD"],["260299","是高侧信号"],["261250","CANH"],["262330","与低侧"],["263410","信号"],["264490","CANL"],["265570","之差。"],["266740","逻辑值"],["267244","1"],["267748","由低"],["268252","VD"],["268756","表示，"],["269260","称为隐性状态。"],["273400","逻辑值"],["273904","0"],["274408","由高"],["274912","VD"],["275416","表示，"],["275920","称为显性状态。"],["279700","驱动器可以主动"],["281320","将总线拉至显性状态，"],["282940","但在没有驱动器"],["284935","驱动显性信号时，"],["286930","总线只能通过"],["288460","端接电阻器上的"],["289990","耗散被动返回"],["291670","至隐性状态。"],["293350","我们将在标题为"],["293900","CAN"],["294450","物理层和硬件的"],["295000","TI"],["296190","高精度实验室"],["297380","视频以及标题为"],["298570","CAN"],["298977","协议和"],["299384","CAN"],["299791","FD"],["300198","的"],["300605","TI"],["301012","高精度实验室视频中"],["301420","论述显性和隐性"],["303745","状态的特性及其"],["306070","对消息仲裁的影响。"],["311070","汽车"],["311455","CAN"],["311840","接口"],["312225","由"],["312610","ISO11898"],["312995","标准"],["313380","规定，该标准"],["315945","包括六个部分。"],["318510","每个部分论述此处"],["319110","显示的"],["319710","CAN"],["320310","的某个"],["320910","特定方面。"],["322980","例如，第二部分"],["324760","称为"],["326540","ISO11898-2，"],["328320","其中论述高速"],["329090","CAN"],["329860","的"],["330630","CAN"],["331400","物理层。"],["332170","第五部分在"],["333400","第二部分概述的"],["334630","要求中增加了"],["336055","低功耗模式要求。"],["337480","第六部分概述了"],["340069","部分联网要求。"],["342659","ISO11898"],["344059","标准中"],["345459","使用的命名"],["346860","约定与汽车制造商"],["348884","经常使用的术语类似。"],["350909","很多时候，汽车"],["352019","制造商会使用低速、"],["353130","中速和高速等"],["354190","术语来描述"],["355250","CAN"],["356310","数据速率。"],["359159","这些名称可能"],["360299","相对任意，甚至"],["361440","在不同的汽车制造商"],["363515","之间可能有所不同。"],["365590","可以理解的是，"],["366467","由于"],["367345","ISO"],["368222","标准使用"],["369100","类似的命名规则，因此"],["371195","这些名称可能会引起混淆。"],["373290","低速容错"],["374220","CAN"],["375150","称为"],["376080","LSFT"],["377010","CAN，"],["377940","由"],["378892","ISO11898"],["379845","的"],["380797","第三部分定义，"],["381750","它以最高"],["383130","125"],["384510","千位/秒的速度"],["385890","运行，该速度类似于"],["387030","上面显示的汽车"],["388170","低速"],["389333","CAN"],["390496","定义。"],["391660","不过，对于所有"],["393115","这三种汽车制造商"],["394570","数据速率定义，"],["395950","大多数汽车制造商"],["397330","实际上在实施高速"],["398020","CAN"],["398710","或"],["399400","HS"],["400090","CAN，它们"],["400780","通常以最高"],["402110","1"],["403440","兆位/秒的速度运行，"],["404770","由"],["405665","ISO11898"],["406561","的第"],["407457","2、5"],["408352","和"],["409248","6"],["410144","部分定义。"],["411040","请注意，高速"],["411990","CAN"],["412940","完全覆盖了"],["413890","低速容错"],["415060","CAN"],["416230","的"],["417400","工作范围。"],["418570","TXD"],["419030","和"],["419490","RXD"],["419950","超时"],["420410","时间将"],["420870","CAN"],["421330","收发器的低端"],["424050","范围限制为"],["426770","10"],["427345","至"],["427920","40"],["428495","千位/秒。"],["429070","当前，许多汽车使用"],["430555","传统高速或"],["432040","HS"],["433525","CAN。"],["435010","具有灵活数据"],["435628","速率的"],["436246","CAN"],["436865","或"],["437483","CAN"],["438101","FD"],["438720","是对传统"],["439470","CAN"],["440220","的增强，"],["440970","能将可用宽带"],["442200","增加至高达"],["443430","5"],["445715","兆位/秒。"],["448000","还有许多其他"],["448720","基于"],["449440","CAN"],["450160","的更高层"],["450880","标准和协议，它们"],["452860","决定着各种应用，"],["454840","包括航空、农业、"],["456535","嵌入式控制、"],["458230","工业自动化、"],["459985","军事、船舶和"],["461740","安全关键型应用。"],["463640","这些标准建立在"],["465899","本演示概述的"],["468159","ISO11898"],["469539","标准基础"],["470919","之上，其中许多"],["472300","标准具有决定"],["473500","电磁兼容性"],["474700","和静电放电要求的"],["476595","其他测试标准。"],["478490","要查找更多"],["479075","CAN"],["479660","和"],["480245","CAN"],["480830","FD"],["481415","技术资源"],["482000","以及搜索"],["482994","CAN"],["483988","和"],["484982","CAN"],["485977","FD"],["486971","产品，请访问"],["487965","ti.com/CAN。"],["488960","此外，务必观看我们其他"],["489418","有关"],["489877","CAN、LIN"],["490335","和"],["490794","SBC"],["491252","的"],["491711","TI"],["492170","高精度实验室视频。"],["496080","谢谢观看。"]],"paragraphs":[0],"speakers":{}}