{"words":[["500","大家好，欢迎观看"],["1650","TI"],["2800","高精度实验室。"],["3950","当大家听到时钟和"],["5195","计时系统这两个术语时，"],["6440","会想到什么呢？"],["7910","实际上这涉及很多东西。"],["9830","但是，如何知道"],["11480","哪个时钟最合适呢？"],["13130","本入门培训模块概述了"],["14570","不同时钟和计时功能的"],["17900","应用。"],["19600","红色显示的"],["20360","锁相环和"],["21120","VCO"],["21880","功能"],["22640","是各种时钟"],["23930","解决方案中使用的核心"],["25220","构建块。"],["26690","这些"],["27310","PLL"],["27930","和"],["28550","VCO"],["29170","功能"],["29790","以及关键性能参数"],["30410","在其他高精度"],["31549","实验室培训模块中"],["32689","进行了讨论。"],["34240","什么是时钟？"],["35950","时钟在电子系统中"],["37750","提供脉冲。"],["39550","在信号链中，时钟"],["40735","是关键构建块，"],["41920","可为"],["42940","ADC、DAC、"],["43960","处理器和任何接口媒体"],["44980","提供参考采样计时。"],["48130","任何需要"],["49465","参考时间进行"],["50800","同步、执行命令"],["52585","和传输数据的系统"],["54370","都需要时钟。"],["55600","它们向各种设备"],["56950","提供频率输入，"],["58300","使它们能够"],["59695","执行预期的功能。"],["61090","时钟也可以"],["62290","用作功能块，"],["63490","该功能块将信号源"],["64510","进行倍频和分频，"],["65530","从而扇出特定频率，"],["67460","甚至几个不同的频率。"],["69390","如果系统中"],["70265","需要处理器、"],["71140","高速接口或"],["72580","数据转换器，"],["74020","则需要时钟解决方案。"],["76240","我们先来介绍"],["76847","最常用的功能"],["77455","-"],["78062","晶体"],["78670","振荡器。"],["79570","关键参数"],["79982","是以"],["80395","PPM"],["80807","度量的"],["81220","振荡频率和"],["82870","精度，及以抖动或"],["84520","相位噪声度量的信号质量。"],["87789","图中显示了简化的"],["89920","晶体输入电路。"],["91510","晶体连接在"],["93040","逆变器的输入和输出之间，"],["94570","其中，R"],["95387","sub"],["96205","S"],["97022","是一个串联电阻，"],["97840","用于在需要时降低驱动电平。"],["99700","芯片内部的"],["100494","有源电路"],["101289","会产生一个"],["102519","正反馈回路"],["103750","该回路也称为"],["105489","负电阻，用来提供刺激，"],["107229","使晶体开始"],["108744","并维持振荡。"],["110259","由于晶体的"],["111429","高机械共振"],["112599","(q)，"],["113770","仅允许特定的"],["115210","频率振荡，"],["116650","这取决于晶体的切割。"],["118303","通常，这将在小于"],["118942","100MHz"],["119581","的频率范围内，"],["120220","最常见的基本共振"],["121900","小于"],["123186","40MHz"],["124473","左右。"],["125760","负载电容"],["126610","CL1"],["127460","和"],["128310","CL2"],["129160","用于控制晶体的"],["130870","初始频率精度。"],["132420","输出类型可以是"],["133775","单端或差分。"],["135130","参考振荡器的"],["136060","不同风格可以推断出"],["136990","精度和稳定性。"],["139220","TCXO"],["140375","经过温度补偿，"],["141530","在工作温度范围内"],["142690","具有低"],["143850","PPM。"],["145010","OCXO"],["145886","包括用于"],["146763","保持温度的烤箱"],["147640","或加热器，并在"],["149260","整个温度范围内"],["150880","具有更低的"],["151479","PPM。"],["152079","我们还可以添加"],["152904","电压控制"],["153730","来调整"],["154336","VCXO"],["154942","或"],["155548","VCTCXO"],["156154","中的"],["156760","负载、电容和频率。"],["159550","压控振荡器"],["160330","在某些方面"],["161110","类似于"],["161875","VCXO。"],["162640","但"],["163315","VCO"],["163990","通常"],["164665","具有更高的频率和"],["165340","更宽的调谐范围。"],["167230","参考振荡器"],["167792","和"],["168355","VCO"],["168917","都是"],["169480","锁相环的组件。"],["171490","并且它们各自产生的噪声"],["172255","相加形成整体"],["173020","PLL"],["173785","噪声。"],["174550","几乎所有"],["175750","电子系统中都有"],["176950","实时时钟"],["178120","(RTC)。"],["179290","大家可以"],["180040","将它想象为"],["180790","上一张幻灯片中"],["181825","晶体振荡器的"],["182860","低功耗实现。"],["184272","诀窍是在不影响"],["185126","太多频率精度的"],["185980","情况下尽可能减少电流。"],["189280","RTC"],["189940","通常以"],["190600","32KHz"],["191260","运行，"],["191920","功耗在微安范围内，"],["194200","但"],["195140","PPM"],["196080","精度可能较低，"],["197020","以每天的秒数度量。"],["199480","许多应用中"],["200995","都使用了计时器，"],["202510","但最常用于"],["204145","电池供电的电路，"],["205780","尤其是备用电池"],["207295","需要延长使用寿命时。"],["208810","没有人希望"],["210355","电池意外地没电。"],["211900","对于计时器，可以向"],["213475","内部振荡器添加一些逻辑，"],["215050","并且计数器"],["216555","将以毫秒或分钟进行倒计时。"],["218060","一旦计数器为空"],["219210","且计时器到期，"],["220360","将提供唤醒信号。"],["222800","此技术允许"],["224010","关闭整个系统，"],["225220","并在几分钟或几小时后"],["226795","唤醒控制器"],["228370","以执行管理任务"],["230275","或开始正常运行。"],["232180","睡眠电流可以"],["233335","大幅降低至"],["234490","纳安范围。"],["235900","睡眠时间"],["237070","在看门狗计时器中非常重要，"],["238240","因为它也会影响"],["239155","整个系统的"],["240070","电流消耗。"],["241570","如果系统具有处理器、"],["243020","高速"],["244470","I/O、"],["245920","通信或物理层"],["246715","连接，"],["247510","则将需要多个"],["248425","时钟频率"],["249340","来支持这些"],["250600","处理和通信"],["251860","网络。"],["253090","还有一些"],["253860","IC"],["254630","时钟解决方案"],["255400","具有更高的"],["256135","集成度，"],["256870","可以以更低的"],["258130","制造材料成本和"],["259390","更高的可靠性"],["261336","提供类似的功能。"],["263283","当需要"],["264116","单个频率的"],["264950","多个副本时"],["265752","（例如"],["266555","25MHz"],["267357","需要四次），"],["268160","或者可能需要"],["268940","8"],["269720","个"],["270500","时钟频率为"],["271280","100MHz"],["272400","的信号，"],["273520","那么"],["274640","时钟缓冲器可能比"],["275282","多个"],["275925","XO"],["276567","更适合。"],["277210","时钟缓冲器"],["279015","（也称为扇出）"],["280820","接收输入，并将"],["282215","输入频率的副本"],["283610","扇出到多个输出。"],["285220","时钟缓冲器通常"],["286017","可以有"],["286814","1-n"],["287611","个输出，"],["288409","其中，n"],["289004","为"],["289599","2，"],["290194","最多可以达到"],["290789","1-12，甚至"],["291384","1-20。"],["294680","在简单的扇出"],["295615","缓冲器中，通常需要的是"],["296550","抖动极低或"],["297975","解决方案成本低，"],["299400","以及较低的输出到输出偏斜。"],["302188","与晶体"],["302959","振荡器相似，"],["303730","有差分和"],["304940","单端输出类型，"],["306150","以及可以提供灵活性"],["307545","和性能的"],["308940","其他选项。"],["310140","在通用缓冲器中，"],["311655","与差分形式一样，"],["313170","希望获得更高的性能。"],["315810","而且，"],["317415","除了附加抖动中的偏斜之外，"],["319020","传播延迟和"],["320805","可能的延迟变化等规范"],["322590","可能也很重要。"],["324290","还需要一种"],["325085","配置功能的方法，"],["325880","例如"],["327030","I2C、"],["328180","窥探或引脚控制，"],["329330","以选择所需的"],["330365","输入/输出类型"],["331400","和"],["332045","I/O"],["332690","电压电平，"],["333335","以适应系统"],["333980","需求。"],["335240","支持的典型格式"],["336248","包括"],["337256","LVCMOS、LVDS"],["338265","和"],["339393","LVPECL、HCSL"],["340521","等。"],["341650","现在，通常情况下，"],["342810","系统需要"],["343970","比简单的扇出缓冲器更多的资源"],["345670","来支持多个频率。"],["347370","例如，"],["347876","如果需要"],["348383","25MHz、"],["348890","100MHz"],["350240","和"],["351590","156.25MHz，"],["352940","该怎么办？"],["354330","时钟发生器是"],["355510","一种特殊的电路，"],["356690","可通过"],["358130","一个或多个锁相环"],["359570","从单个参考输入"],["361265","产生多个频率输出。"],["362960","时钟发生器采用"],["364370","激励或参考输入，"],["365780","可以是晶体、"],["366860","振荡器或"],["367940","时钟树上一级的"],["369740","时钟输出，并从中产生"],["371540","多个频率"],["372845","或所需"],["374150","相同频率的"],["375448","多个副本。"],["376746","锁相环"],["377754","(PLL)"],["378762","是一种反馈系统，"],["379770","在此系统中，VCO"],["381000","跟踪"],["382230","参考输入的"],["383460","相位和频率。"],["384720","因此，"],["385560","VCO"],["386400","输出频率"],["387240","是相位检测器频率"],["388935","乘以时间。"],["390630","有关"],["391200","PLL"],["391770","和"],["392340","VCO"],["392910","构建块的更多详细信息，"],["393480","请访问高精度实验室"],["394860","锁相环基础知识"],["396240","培训系列。"],["397590","时钟发生器中的"],["398500","每个输出分频器"],["399410","D"],["400320","可以选择一个"],["401270","PLL，"],["402220","对其进行分频并产生"],["403170","输出频率。"],["404730","有时，多个输出"],["405810","组合在一起"],["406890","并共享一个公共的"],["407820","输出分频器。"],["408750","在这种情况下，这些"],["409605","输出将始终"],["410460","具有相同的时钟频率。"],["412750","为什么需要时钟发生器？"],["415200","当系统用例"],["416340","（例如网络和工厂"],["417480","自动化，也可能是"],["418935","医学成像）"],["420390","需要不同的"],["421530","时钟频率时，"],["422670","与使用"],["423735","多个振荡器"],["424800","和/或晶体相比，"],["426245","时钟发生器更合适。"],["427690","为便于"],["428770","以后讨论，"],["429850","我们将输出缓冲器分频器"],["431605","称为"],["433360","时钟分配块。"],["435190","以不同的方式"],["436435","查看时钟操作，"],["437680","可分为三种主要的"],["439510","模拟时钟架构。"],["441340","这里显示的是简化框图，"],["442915","显示了"],["444490","时钟分配网络中的参考。"],["446590","时钟分配"],["447805","或时钟缓冲器"],["449020","不过滤任何噪声。"],["450310","它只能增加抖动。"],["451870","但这是简单且低功耗的。"],["454240","时钟发生器中"],["455350","常见的单环路"],["456460","在同一步骤中"],["457825","同时进行抖动消除"],["459190","和倍频。"],["460659","由于"],["461025","PLL"],["461391","VCO"],["461757","工作，"],["462123","单环路"],["462490","的确为"],["463170","大于"],["463850","10KHz"],["464530","的更高频率噪声"],["466060","提供了参考"],["467590","滤波。"],["468980","但是，双环路"],["469905","或级联环路"],["470830","将在更接近载波的"],["472435","频率偏移处"],["474040","更好地清除抖动，"],["475675","因为它将在"],["477310","第一个抖动清除"],["477873","PLL"],["478436","中"],["479000","使用"],["479563","VCXO"],["480126","晶体振荡器。"],["480690","第一个"],["481280","PLL"],["481870","(PLL1)"],["482460","应该"],["483050","具有较窄的环路带宽，"],["483640","以滤除"],["484705","参考噪声。"],["485770","第二个"],["486490","PLL"],["487210","(PLL2)"],["487930","应该"],["488650","具有较宽的环路带宽，"],["489370","以利用"],["490815","清除抖动后的参考噪声。"],["492260","第二个"],["493007","PLL"],["493755","执行更多的"],["494502","倍频功能，"],["495250","以允许"],["496675","分配块分频为"],["498100","所需的"],["499600","输出频率。"],["501100","例如，"],["502195","如果想使用恢复的[听不清]时钟"],["503290","作为输入参考时钟，"],["504767","或者需要"],["506245","在载波附近"],["507182","产生低相位噪声，"],["508120","则在参考输入"],["509120","噪声较大的情况下，"],["510120","将使用双级联"],["511610","环路架构，"],["513100","因为典型的"],["513736","VCO"],["514372","在"],["515008","10KHz"],["515644","以下的"],["516280","近端相位噪声性能"],["517645","较差。"],["519010","当输入和输出"],["520270","频率的整数关系"],["521530","不佳时，可能还需要"],["522865","使用抖动清除器。"],["524200","例如，如果"],["525480","参考频率为"],["526760","12.288MHz，"],["528040","而"],["528706","VCO"],["529372","的参考频率"],["530038","为"],["530704","2.5GHz，"],["531370","则将导致非常低的"],["532260","32KHz"],["533150","相位检测器"],["534040","频率。"],["535660","较高的相位检测器"],["536650","比较频率"],["537640","通常会改善"],["538530","PLL"],["539420","性能。"],["540310","双环路可以为"],["541172","第二个"],["542035","PLL"],["542897","提供"],["543760","10MHz"],["544345","或"],["544930","100MHz"],["545515","的参考输入，"],["546100","这是比较频率的"],["547270","300"],["548440","或"],["549610","3,000"],["550360","倍。"],["551110","需要同步"],["552925","多个频率源，"],["554740","以在输入和"],["556615","多个频率输出之间"],["558490","提供确定的相位关系。"],["561220","通常，抖动清除器"],["562435","将在分配路径中"],["563650","包括"],["564790","延迟补偿网络，"],["565930","以帮助"],["566980","平衡输出之间的"],["568030","任何路由差异。"],["569770","实际上，"],["570610","对于"],["571450","时间紧迫的应用，"],["572830","同步变得越来越重要。"],["574210","为了实现此功能，"],["575650","网络同步器"],["577090","是关键组件，"],["578035","通常用于"],["578980","满足一些"],["579665","更具挑战性的"],["580350","ITU"],["581035","和"],["581720","电信标准。"],["582710","许多"],["583308","ITU、电信"],["583906","和"],["584504","4G、5G"],["585102","标准"],["585700","都要求"],["586615","始终保证"],["587530","时间和频率同步。"],["590410","网络同步器"],["592135","始终提供"],["593860","高度稳定的时钟，"],["595360","而不管是否存在"],["596860","参考输入。"],["597940","基于合格性和优先级，"],["599185","以无中断的方式"],["600430","监视和切换"],["602665","冗余输入，"],["604900","并且相位干扰非常低。"],["607510","数字锁相环"],["608300","(DPLL)"],["609090","可在"],["609880","参考丢失时"],["611245","提供保持功能，"],["612610","并可进行编程"],["613450","以使环路带宽"],["614290","小于"],["615070","1Hz。"],["615850","想象一下，"],["616630","要在模拟域中"],["617410","达到低于"],["618565","1Hz"],["619720","的带宽，"],["620875","需要一个电容器。"],["622030","频率输出"],["623002","跟踪参考近端的"],["623975","稳定性。"],["626050","DPLL"],["627380","带宽"],["628710","决定了长期漂移方面和"],["630040","相位瞬变。"],["632080","XO"],["632848","和"],["633616","APLL"],["634384","决定了"],["635152","短期时钟方面、"],["635920","相位噪声和杂散。"],["638230","混合信号技术"],["640080","用于获得出色性能。"],["641930","但是，片上"],["643736","LCVCO"],["645543","通常会带来一些限制。"],["647350","一种"],["648265","将体声波"],["649180","(BAW)"],["650095","振荡器"],["651010","集成到"],["652300","网络同步器的新架构"],["653590","采用了"],["654226","DPLL"],["654862","和"],["655498","APLL"],["656134","的主要优势，"],["656770","并将它们"],["657610","组合在一起，"],["658450","从而降低了带内噪声。"],["660423","通常，只有"],["660895","低频"],["661367","XO"],["661840","足以实现小于"],["663050","100"],["664260","飞秒的抖动。"],["665470","本培训视频"],["666925","到此结束。"],["668380","谢谢观看。"],["669840","我们设置了一个包含"],["670715","五个问题的简单测验，"],["671590","请完成该测验，检验您对"],["673135","视频内容的理解程度。"],["674680","如果您需要有关"],["675840","TI"],["677000","时钟和计时产品的"],["678160","更多信息，请访问"],["682450","ti.com/clocks。"],["698410","我们来核对一下答案。"],["700206","第一个问题的答案是“错误”。"],["701710","时钟发生器、"],["702775","抖动清除器"],["703840","或网络同步器可以"],["705175","从单个参考"],["706510","提供多个频域。"],["709110","第二个问题的答案是“正确”。"],["711227","所有这些功能"],["712018","都可以包含在"],["712810","时钟分配块中，"],["714295","并且始终至少"],["715780","存在一个输出缓冲器。"],["718570","第三个问题的答案是“错误”。"],["721120","由于时钟缓冲器"],["722085","复制了输入，"],["723050","因此不会引入"],["724255","频率误差。"],["725460","偏斜用于衡量输出"],["727690","之间的相位差。"],["729920","第四个问题的答案是“正确”。"],["730970","PLL1"],["731852","的环路带宽较窄，"],["732735","可滤除参考源的噪声。"],["734360","PLL2"],["736160","执行倍频，"],["737960","允许分配块"],["739430","分频为所需的"],["740900","输出频率。"],["742580","最后一个问题的"],["744045","答案也是“错误”。"],["745510","无论是在参考"],["747270","之间切换还是"],["749030","进入没有参考的"],["750230","保持模式，网络同步器"],["751430","都可以保持"],["752885","时间和频率精度。"],["754340","因此，对于参考是否稳定"],["755240","或是否进出基本不受影响。"],["756140","the"],["756578","reference"],["757017","is"],["757456","stable"],["757895","or"],["758334","goes"],["758773","in"],["759212","and"],["759651","out."]],"paragraphs":[0],"speakers":{}}