{"words":[["2640","您好。"],["3270","歡迎收看"],["4125","TI"],["4980","精密實驗室，"],["5835","今天的主題是控制器"],["6690","區域網路通訊，"],["7770","通常又稱為"],["8850","CAN"],["9930","通訊。"],["11010","這支影片將會"],["11482","介紹"],["11955","CAN"],["12427","收發器在"],["12900","CAN"],["14390","匯流排中"],["15880","進行通訊的方法，"],["17370","特別是汽車"],["19070","相關應用。"],["20770","本介紹影片內容"],["21697","包含"],["22625","CAN"],["23552","概覽，"],["24480","相關標準介紹，"],["26385","簡單說明實體層，"],["28290","並討論各種"],["29663","CAN"],["31036","通訊協定。"],["32409","這是典型的汽車"],["34314","車體網路範例。"],["36220","中央車身控制或"],["37990","車內任何類似主要"],["39760","裝置都需與"],["41275","車內其他裝置"],["42790","進行通訊，"],["43945","這些裝置通常"],["45100","離主要"],["46270","裝置較遠，"],["47440","才能完成任務。"],["49680","這裡以藍色顯示的"],["50633","CAN"],["51586","匯流排"],["52540","可讓元件彼此在"],["54565","車輛內順暢溝通。"],["56590","以黃色顯示的"],["57780","LIN"],["58970","匯流排則可"],["60160","進一步延伸至周邊裝置。"],["62470","利用此匯流排網路，"],["63805","溫度控制系統"],["65140","便可與電動座椅"],["66445","系統等進行介面溝通"],["67750","以啟動座椅"],["69310","加熱器，"],["70870","或者控制單元"],["72370","可在踩下煞車踏板時"],["73870","啟動煞車燈。"],["76530","此匯流排階層的設計目的"],["78720","在於節省配線成本。"],["80910","配線是車內最"],["82790","昂貴的元件之一。"],["84670","不但重量較重，通常"],["85940","也需以手動方式組裝。"],["87210","因此配線對汽車整體"],["89175","生產成本有非常直接的"],["91140","影響。"],["92700","汽車設計人員利用"],["94200","CAN"],["95700","來減少車內所需配線，"],["97200","降低製造成本"],["99615","並提升燃油效率。"],["102030","CAN"],["103453","是目前汽車最常"],["104876","使用的匯流排。"],["106300","其可讓各種模組，"],["107960","例如電動座椅、"],["109620","車門模組及溫度"],["111265","控制單元等彼此溝通。"],["112910","擁有彈性資料速率"],["113471","的"],["114033","CAN，或稱"],["114595","CAN"],["115156","FD"],["115718","，"],["116280","是在這種匯流排中"],["118380","最常採用的通訊方式。"],["120480","CAN"],["121290","和"],["122100","CAN"],["122910","FD"],["123720","會執行差動雙線"],["124530","介面."],["125850","傳統"],["126574","CAN"],["127299","每秒最高"],["128024","可執行"],["128749","1"],["129474","megabit，"],["130199","CAN"],["130992","FD"],["131786","每秒最高"],["132579","則可執行"],["133373","5"],["134166","megabit。"],["134960","LIN"],["136786","是一種以較低資料"],["138613","速率運作的子匯流排。"],["140440","CAN"],["141746","標準針對多點"],["143053","匯流排應用中異步序列"],["144360","通訊的通訊協定與"],["146280","實體層進行定義。"],["148200","應用設計。"],["149790","每個節點包含一個"],["150492","CAN"],["151194","收發器與"],["151896","MCU"],["152598","中的"],["153300","CAN"],["154590","控制器。"],["155880","通訊會在不同"],["157290","匯流排中發生，"],["158700","其中包括最高每秒"],["159348","1"],["159996","megabit"],["160644","的傳統"],["161292","CAN，"],["161940","以及最高每秒"],["162629","5"],["163318","megabit"],["164007","並具彈性資料速率的"],["164696","CAN。"],["165385","CAN"],["166986","必須與雙絞"],["168588","纜線一起使用。"],["170190","網路應以匯流排拓撲"],["171525","方式進行配線，"],["172860","並盡可能減少"],["174840","短線使用。"],["176820","CAN"],["177558","與"],["178296","CAN"],["179034","FD"],["179772","的"],["180510","匯流排應在兩端"],["181785","以符合網路阻抗的"],["183060","電阻器適當端接。"],["185040","適當端接可幫助"],["186450","減少反射等訊號完整性"],["187860","問題。"],["189480","如果可從匯流排"],["190590","中移除節點，"],["191700","設計人員在選擇"],["193095","終端電阻器位置時"],["194490","必須十分小心。"],["196760","端接可以多種"],["198275","方式達成。"],["199790","標準端接採用"],["201500","匯流排兩端的"],["203210","單一終端電阻器。"],["205250","另一種方式"],["206480","是分裂端接，"],["207710","如右側所示，"],["209495","可提升訊號完整性"],["211280","與電磁放射"],["212825","特性。"],["214370","此外也可消除"],["215300","匯流排共模"],["216230","電壓位準"],["217550","中的波動，"],["218870","同時保持"],["220755","差動波動。"],["222640","CAN"],["223630","的匯流排"],["224620","拓撲與雙絞纜線"],["225610","通常有"],["226720","120"],["227830","歐姆"],["228940","特性阻抗。"],["230050","適當端接通常會需"],["231242","用到"],["232435","120"],["233627","歐姆"],["234820","終端電阻器。"],["237520","由於"],["238055","CAN"],["238591","網路可"],["239127","將"],["239662","CANH"],["240198","與"],["240734","CANL"],["241270","連接到"],["242042","VCC"],["242815","和"],["243587","接地等電源，"],["244360","因此終端電阻器的"],["245680","電源額定值"],["247000","應考慮網路"],["247600","中"],["248200","CAN"],["248800","收發器的"],["249400","短路過電流"],["252145","保護。"],["254890","CAN"],["256059","是一種雙線"],["257229","差動訊號。"],["258399","差分電壓"],["259349","VD"],["260299","是指"],["261250","高側訊號"],["262690","CANH"],["264130","與低側訊號"],["265570","CANL"],["266155","間的差異。"],["266740","低"],["267370","VD"],["268000","代表邏輯值"],["268630","1，"],["269260","指的是"],["271330","隱性狀態，"],["273400","高"],["273904","VD"],["274408","則"],["274912","代表邏輯值"],["275416","0，"],["275920","指的是"],["277810","顯性狀態。"],["279700","驅動器可主動將"],["281320","匯流排拉至顯性狀態，"],["282940","但匯流排只能"],["284935","透過終端電阻"],["286930","中的消耗被動"],["288460","回到隱性狀態，"],["289990","驅動器不會"],["291670","驅動顯性訊號。"],["293350","接下來"],["294175","我們要討論"],["295000","顯性與隱性"],["296785","狀態的特性，"],["298570","以及兩者對"],["299520","TI"],["300470","精密實驗室"],["301420","CAN"],["302001","實體層和硬體及"],["302582","TI"],["303163","精密"],["303745","實驗室CAN"],["304326","通訊協定與"],["304907","CAN"],["305488","FD"],["306070","中訊息仲裁的影響。"],["311070","汽車"],["311647","CAN"],["312225","介面"],["312802","取決於"],["313380","ISO11898"],["315090","標準，"],["316800","其中包含六個部分。"],["318510","每個部分都會處理"],["319110","幾個"],["319710","CAN"],["320310","面向，"],["320910","如此處所示。"],["322980","例如第二部分"],["324760","稱為"],["326540","ISO11898-2，"],["328320","內容包含高速"],["329090","CAN"],["329860","的"],["330630","CAN"],["331400","實體層。"],["332170","第五部分則"],["333400","針對第二部分"],["334630","加入低功率"],["336055","模式要求。"],["337480","部分網路要求則"],["340069","於第六部分說明。"],["342659","ISO11898"],["344059","標準"],["345459","採用的命名慣例"],["346860","與汽車製造商"],["348884","常用詞彙類似。"],["350909","汽車製造商"],["352019","常會使用"],["353130","低速、中速和"],["354720","高速等詞彙"],["356310","來描述"],["357259","CAN"],["358209","資料速率。"],["359159","這些名詞"],["360299","相對比較隨意，"],["361440","甚至在不同汽車製造商"],["363515","間可能會有所不同。"],["365590","這些名詞自然"],["367345","會造成混淆，"],["369100","因為"],["370147","ISO"],["371195","標準使用"],["372242","類似的命名方式。"],["373290","低速容錯"],["374220","CAN，"],["375150","又稱"],["376080","LSFT"],["377010","CAN，"],["377940","由"],["378892","ISO11898"],["379845","第三"],["380797","部分進行定義，"],["381750","可以最高每秒"],["382785","125"],["383820","kilobit"],["384855","運行，"],["385890","此速度與上方的"],["386460","低速"],["387030","CAN"],["387600","汽車"],["388170","定義類似。"],["391660","但就這三種汽車"],["393115","製造商資料速率定義"],["394570","而言，多數"],["395950","汽車製造商"],["397330","實際上執行高速"],["398020","CAN，"],["398710","或稱"],["399400","HS"],["400090","CAN，"],["400780","通常可以最高每秒"],["401777","1"],["402775","megabit"],["403772","的速度運行，"],["404770","並由"],["405665","ISO11898"],["406561","第"],["407457","2、"],["408352","5"],["409248","和"],["410144","6部分加以定義。"],["411040","請注意高速"],["411990","CAN"],["412940","與低速"],["413890","容錯"],["415060","CAN"],["416230","的"],["417400","運作範圍完全重疊。"],["418570","CAN"],["419030","收發器"],["419490","因"],["419950","TXD"],["420410","和"],["420870","RXD"],["421330","逾時時間，以"],["422236","每秒約"],["423143","10"],["424050","到"],["424956","40"],["425863","kilobit"],["426770","受限在低端。"],["429070","目前許多汽車採用"],["430555","傳統高速或"],["432040","HS"],["433525","CAN。"],["435010","擁有彈性資料速率"],["435752","的"],["436494","CAN，或稱"],["437236","CAN"],["437978","FD，"],["438720","是傳統"],["439282","CAN"],["439845","的"],["440407","強化版，"],["440970","可將可用頻寬"],["442200","提升到高達"],["443430","每秒"],["444953","5"],["446476","megabit。"],["448000","另外還有許多"],["448960","較高層"],["449920","CAN"],["450880","標準與通訊協定"],["452860","可管理應用，包含"],["454840","航空、農業、"],["456535","嵌入式控制、"],["458230","工業自動化、"],["459985","軍事、海事與"],["461740","重要安全應用。"],["463640","這些標準都以本簡報"],["464769","提到的"],["465899","ISO11898"],["467029","標準"],["468159","為基礎，其中"],["470229","很多透過其他"],["472300","測試標準來"],["473500","管理電磁"],["474700","功能和靜電"],["476595","放電要求。"],["478490","若想進一步了解"],["479075","CAN"],["479660","和"],["480245","CAN"],["480830","FD"],["481415","技術資源，"],["482000","並搜尋"],["482870","CAN"],["483740","與"],["484610","CAN"],["485480","FD"],["486350","產品，"],["487220","請造訪"],["488090","ti.com/CAN。"],["488960","此外，請記得觀賞"],["489762","其他"],["490565","TI"],["491367","精密實驗室的"],["492170","CAN、LIN"],["493147","和"],["494125","SBC"],["495102","相關影片。"],["496080","謝謝收看。"]],"paragraphs":[0,125850],"speakers":{}}