The TPS7B4260-Q1 is a monolithic, integrated, low-dropout (LDO) voltage tracker. The device is available in an 8-pin HSOIC package. The TPS7B4260-Q1 is designed to reliably provide power to off-board sensors with a wire harness, even in harsh automotive environments. In such severe operating conditions, the cables in the harness are potentially exposed to various fault conditions, increasing risk of failure. Such conditions include short to ground, short to battery, and overtemperature. The TPS7B4260-Q1 comes with integrated protection features against each of these fault conditions, as well as protection against reverse polarity. The device incorporates a topology containing two back-to-back P-channel metal-oxide semiconductor field-effect transistors (MOSFETs). This PMOS topology eliminates the need for an external diode that is otherwise required to prevent the flow of reverse current. The high 300mA current rating of the device potentially allows a single tracker to power multiple off-board sensors simultaneously. The device is designed to handle a 45V (absolute maximum) input voltage and survive the automotive load dump transient conditions.
The TPS7B4260-Q1 provides a protective buffer for the ADC and MCU against fault conditions, while securely transferring power to the off-board sensors. A reference voltage applied at the adjustable input pin (ADJ/EN) is tracked with a very tight 6mV (max) tolerance at the FB pin. This tolerance holds true for all variations across the specified line, load, and temperature values. For ratiometric sensors whose output is sampled by the ADC, this tight tracking tolerance is particularly benficial. This tolerance makes sure that the error between the ADC full-scale reference and the sensor power-supply voltage is minimal. The ratiometricity of the sensor measurement is thereby maintained.
Output voltage becomes equal to the voltage at the ADJ/EN pin (± the tracking tolerance) by tying the FB pin directly to the OUT pin. If the ADC full-scale reference voltage equals the sensor supply voltage, connect the reference voltage directly to the ADJ/EN pin. If the sensor supply is lower than the reference, use a resistive divider at the ADJ/EN pin. This divider helps scale down the reference voltage to match the sensor supply voltage. If the sensor supply is higher than the reference, use a resistive divider between the FB and OUT pins. This divider helps scale up the ADC full-scale reference voltage and match the sensor supply voltage.
By setting the ADJ/EN input pin low, the TPS7B4260-Q1 switches to standby mode. In this mode, the quiescent current consumption of the LDO reduces to less than 3.8μA.
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NAME | DDA | ||
ADJ/EN | 5 | I | Adjustable/enable input pin. Connect the external reference voltage to this pin. This pin connects to the inverting input of the error amplifier internally. A low signal below VIL disables the device, and a high signal above VIH enables the device. Connect the voltage reference directly, or with a voltage divider to attain output voltages lower than the reference. To compensate for line influences, place a 0.1μF capacitor close to this pin. |
DNC | 2 | — | Do not connect a voltage source to this pin. Either leave the pin floating or connect to GND to improve thermal performance. |
FB | 4 | I | Feedback pin. This pin is connected to the noninverting input of the error amplifier internally and controls the output voltage. For output voltages equal to or less than the external reference voltage, connect this pin directly to the output pin. To attain output voltage values higher than the reference, use a voltage divider with external feedback resistors. |
GND | 6, 3 | G | GND pin. Connect this pin to a low impedance path to ground. |
IN | 8 | I | Input power-supply voltage pin. For best transient response and to minimize input impedance, use the recommended value or larger ceramic capacitor from IN to GND. See the Recommended Operating Conditions table. Place the input capacitor as close to the input pin of the device as possible to compensate for line influences. See the Input and Output Capacitor Selection section for more details. |
NC | 7 | — | Not internally connected. For best thermal performance, connect these pins to GND. |
OUT | 1 | O | Regulated output voltage pin. A capacitor is required from OUT to GND for stability. Select a ceramic capacitor within the range of COUT values provided in the Recommended Operating Conditions table. Place this capacitor as close to output of the device as possible. See the Input and Output Capacitor Selection section for more details. |
Thermal Pad | Pad | Thermal pad. Connect the pad to GND for best possible thermal performance. |
MIN | MAX | UNIT | ||
---|---|---|---|---|
VIN | Unregulated input pin voltage | –40 | 45 | V |
VOUT | Regulated output pin voltage | –5 | 45 | V |
VIN - VOUT | Input-Output Differential | -45 | 45 | V |
VFB | Feedback pin voltage | –5 | 45 | V |
VADJ/EN | Adjustable reference and enable pin voltage | –40 | 45 | V |
TJ | Operating junction temperature | –40 | 150 | °C |
Tstg | Storage temperature | –65 | 150 | °C |