All trademarks are the property of their respective owners.
Unlike the ideal operational amplifier, real operational amplifiers have input and output limitations that dictate a realistic range of values of where they can operate and remain working in a linear state.
In the case of current sensing amplifiers, the typical input restriction of the standard operational amplifier is removed. This is due to an internal topology of input stage transistors that allows for common mode voltages far in excess of the supply voltage(s). This common mode voltage is rejected,the differential voltage is level shifted down, and is then processed by the output stage. The ability of such a front end is useful in various scenarios, from the avoidance of additional components for level shifting data for operation by an analog to digitial converter, avoiding additional supply voltages simply for biasing operational amplifiers, and many more.
However, when discussing the output structure of a current sense amplifier, the output stage typically contains design constraints that must be taken into account for the device to operate linearly. Typically, current sense amplifiers employ CMOS type output stages, which display a small amount of swing loss as the demand for load current increases. These restrictions are made apparent in the datasheet, and reside in a graph commonly referred to as a "claw" curve.
A mistake that is often made with regard to swing limitations is that they are treated as a static condition, if considered at all. Commonly, swing test conditions can often be found in the Electrical Characteristics table of a current sense amplifier data sheet, such is in Figure 2-1.
Examining this information from the INA240 High- and Low-Side, Bidirectional, Zero-Drift, Current-Sense Amplifier With Enhanced PWM Rejection Data Sheet, several observations are obtained. First, the output of the amplifier is not ideal to the supply, but rather is only capable of swinging to 4.8 V in the worst case (4.95 V typical) condition for a supply of 5 V. The same observation is also made regarding the device's ability to swing to GND. This information demonstrates that, should the device be operated in a unidirectional manner, that is, the REF pins of the INA240 both set to GND, that the output is not capable of truly measuring 0 A. (A true drive to 0 A is possible in a unidirectional setup, however, if the reference is used to pedestal above the swing condition. This comes at the loss of a small amount of dynamic range.)
These conditions do not hold true for the entirety of the potential load range, however. As required load current increases, this often comes at the expense of output swing head room of the device. The conditions above only examine swing on the output of the device in a single location for potential loading, in this case 10kΩ to GND. Should the loading of the output change, and more current is demanded, this can potentially alter the output stage's swing characteristics, and lead to saturation against the rail if not properly designed for. A good example to imagine here is a step in load current at the output of the current sense amplifier. The designer needs to ensure that the largest load current is taken into account with respect to desired full scale range to ensure that the output of the device is capable of handling this change.
Load resistance and the maximum desired output voltage for the output stage allow the engineer to calculate the maximum current required by the load. For example, in the data sheet test condition discussed above, the maximum output capable is 4.8 V, and the load resistance is 10 kΩ. If a design were in motion with these desired parameters, then maximum current sourced by the output can be calculated as:
For the Texas Instruments' amplifier portfolio, this information across the load current range is typically conveyed in a common figure referred to as the "claw" curve, as they somewhat resemble animal claws. Figure 2-2 shows the claw curve of the INA240.
These curves are normally divided into a top and bottom section, and the above curve is no different. The upper family of curves demonstrates the devices ability to source current, while the lower family of curves gives the device's ability to sink current. Information is also provided at the ambient temperature point, and the extremes of the device's temperature range. Some devices may include additional temperature curves, but these three datasets will normally be provided at a minimum.
Breaking down the curves, you can again make several observations. First, it can be seen that as the desired load current grows, the ability of the device to swing completely to the rail diminishes. This is due to the fact that, for CMOS output stages, as load current increases through the FET, and a drop is created over the RDS(ON) of the FET that will scale with the output current of the device. This is visualized in a high level diagram in Figure 2-3.
Next, this relationship is not linear across the entire range, and a portion of the curve is reached where significant falloff is observed. This is due to the fact that the RDS(ON) of the FETs is not a linear process, and increases with increasing current from drain to source.
Finally, an important aspect of these curves to understand is that these curves are not meant to be interpreted as a simple "translational" relationship as the claw curve limit is reached. Typically, a good design rule is to provide some amount of headroom away from the hard limit of the claw curve. While amplifier output stages are relatively linear to a point, there are diminishing returns as the rail is approached, and components of both the linear area and saturation area will be present in the output. Figure 2-4 shows a typical FET curve is demonstrated to help visualize this in .
For this reason, it is typically recommended that a small amount of margin be built into the design to work away from the hard value shown in the claw curve, nominally a few tens to hundreds of millivolts.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS. |
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources. |
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products. |
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2020, Texas Instruments Incorporated |