Design Goals
The design goal is the realization of
a high-side, bidirectional current sensing circuit using a unidirectional current
sense amplifier.
| Input |
Output |
Supply |
Error |
| IMin |
IMax |
Vout, min |
Vout, max |
VS |
Output Error |
| –10 A |
+10 A |
50 mV |
4.8 V |
5 V |
≤ 2% |
Design
Description
This circuit
utilizes a TL1431, 2N2222A NPN transistor (see the following image), and passive
components to achieve bidirectional sensing from a unidirectional current sense
amplifier, the INA293. In this particular setup, the normal operating load is from
–10 A to 10 A, with a supply voltage of 5 V. This topology may be used for any
supply voltage independent of the desired offset. The solution presented in this
circuit is a high-side implementation, with a common-mode voltage range of 2.5 V to
110 V.
Design Notes
- This topology is meant for
high-side implementation, where the IN+ and IN– pin of the INA293 are referenced
to the common-mode voltage (VCM) of the application. While this
circuit is capable of withstanding the full 110-V common mode of the INA293, a
limitation exists on the lower end, and VCM must be held
> 2.5 V. This is due to reference of the TL1431
of 2.5 V, and the need for the current flow to sink towards the TL1431 for
proper offset voltage creation. Therefore, the common-mode voltage of the IN–
pin must be
> 2.5 V to ensure valid
operation.
- For the presented design, a 24
VCM is considered, and the 2N2222A is chosen to complete the
design based on these parameters. A BJT possessing greater VCE
capabilities is needed for high-voltage applications
> 50 VCM.
- While this circuit provides the
ability to measure in multiple directions, it does not change the fact that the
INA293 is inherently a unidirectional device. This infers that one direction of
current sensing will be more accurate than the other, as one direction will
measure towards the offset voltage of the device, leading to increased error in
this direction. The effects of this may be mitigated in part by the use of a
one-point calibration, and is discussed later in this document.
Design Steps
- Design the Offset Current:
The offset current ultimately flows over R1 to create the referred to input
(RTI) offset sense voltage, and is determined by resistor R2. The default
reference voltage of the TL1431 is 2.5 V, and here, a 1-kΩ resistor is chosen,
and the offset current is calculated as shown in the following equation:
- Design RTI Offset Voltage
Point: With IOFFSET determined in the previous equation, R1
may now be selected to determine the reference point of the design
(VREF). This point needs to be chosen based on where the origin
of the output to be located is wanted. This is typically influenced by
swing-to-rail limitations, as well as the defined linear operating region for
the device in question. From the gain error specification of the INA293, the
linear operating region is defined as from 50 mV above GND, to 200 mV below
supply, and this is chosen to be the limiting bounds of the design to maximize
accuracy. For these points, a roughly equidistant VREF of 2.4 V was
chosen, but actual resistor selection of R1 (48.7 Ω from the ideal 48 Ω)
ultimately led to a 2.435-V design. This point is determined by the following
equations:
- Choose RSHUNT to
Optimize Input Range: With the RTI Offset designed, a shunt may now be
chosen for the desired sensing range, taking the constant RTI offset voltage
into account. For the desired lower bound of 50 mV, this correlates to a 2.5-mV
sense voltage referred to the input pins of the INA293, while the upper bound
correlates to 240 mV. From the desired bound design targets, for the A1 variant,
it is calculated that the maximum allowable shunt to achieve this goal is found
using the following:
Using
the lesser of these values, this shows that a maximum 11.825-mΩ shunt may be used to
satisfy the upper bound, and some small truncation of the lower region should be
expected. Choosing a convenient standard value resistor, 10 mΩ was selected to
complete the design. The final input VSENSE swing is calculated as:
The expected corresponding output is found using:
The designed outputs are found to be within the linear
operating range, but fall short of utilizing the full dynamic range here. The reason
for this is due to the choice of sense resistor of 10 mΩ versus the defined maximum
of 11.8 mΩ. Range may be increased further, but this will often come at the tradeoff
of increased BOM cost for custom values, or additional components to form parallel
combinations that achieve a closer target to the theoretical maximum.
- Verify shunt derating is
sufficient: A necessary aspect of proper shunt design is ensuring that
the design choice has sufficient margin for power derating. As the device heats
in the environment, the amount of power the shunt is capable of dissipating is
derated by a certain factor. For continuous sensing, this factor can be as high
as 0.6. Taking this into account, for the design, a shunt must be chosen that is
rated for at least the following:
So for a successful design, a shunt of at least 2 W rated power is chosen for
continuous sensing.
- Choose the correct BJT NPN
transistor: Dependent on the common modes expected to be seen by the
application, a corresponding BJT must be chosen to be able to withstand this
VCM. The voltage ultimately seen by the BJT is calculated as in the following
equation:
Add some margin for any potential voltage transients on the common mode. For the
given design, the 2N2222A is chosen, as it is able to withstand a VCE of 50 V
maximum, and meets the needs of the design. The expected power dissipated through
the BJT is found with the following equation:
- Examine Error. Calibrate if
necessary: As discussed in previous sections, it is expected that the
current sense amplifier will be more accurate in the direction of measurement as
the output is driven toward supply. Less accurate measurements are expected as
the sense voltage decreases, and errors from the offset voltage begin to have
more effect. A remedy for this is to perform a one-point calibration in logic to
reduce the effects of the offset voltage, if necessary. Here, the design is
within the design goal, so this is not necessary.
Design Simulations and Calculations
DC Sweep Results, –10 A <
ILOAD < 10 A
The following
Root-Sum-Square (RSS) error curve was generated for the following resistor
tolerances and RSS equation:
- RSHUNT = ±0.1%
- R1 = ±1%
- R2 = ±1%
Note that more accurate resistors will result in
further reduction of the total error curve.
Design References
See Analog Engineer's Circuit Cookbooks for TI's comprehensive
circuit library.
Download the PSpice files for this circuit – SBOA545.
For more information on the INA293
device, see the INA293 –4-V to 110-V, 1-MHz, High-Precision Current Sense
Amplifier data sheet.
Additional Resources