The effect of heavy-ion irradiation on the single-event effects performance of the radiation-tolerant TRF0208-SEP is summarized in this report. Heavy-ions with an LETEFF up to 56.1 MeV-cm2/mg were used to irradiate three production devices in 12 runs. Flux up to 106 ions/cm2-s and fluences up to 107 ions/cm2 at temperatures of 25°C (SET) and 125°C (SEL), were used for the characterization. Results demonstrate that the TRF0208-SEP is SEL-free up to LETEFF = 56.1 MeV-cm2/mg and 125°C, and the cross section for the SET is discussed.