This report covers the radiation characterization results of the
SN54SC4T125-SEP radiation tolerant, single power supply quadruple buffer translator
gate. The study was done to determine Total Ionizing Dose (TID) effects under high
dose rate (HDR) up to 50 krad(Si) as a one time characterization. The results show
that all samples passed within the specified limits up to 50 krad(Si). Radiation Lot
Acceptance Testing (RLAT) will be performed using five units at a dose level of 30
krad(Si) for future wafer lots per MIL-STD-883 TM 1019.
The SN54SC4T125-SEP is packaged
in a space enhanced plastic for low outgassing characteristics and is Single
Event Latch-Up (SEL) immune up to 43 MeV-cm2 / mg, which makes the
device an option for low Earth orbit space applications.
The SN54SC4T125-SEP Total
Ionizing Dose (TID) Report covers the TID performance of all seven devices
listed below. The SN54SC4T125-SEP device covers all functional blocks and active
die area of the other six devices, which is why the device was selected for
total ionizing dose testing for this group of logic gate devices.
- SN54SC4T125-SEP
- SN54SC3T97-SEP
- SN54SC3T98-SEP
- SN54SC4T00-SEP
- SN54SC4T02-SEP
- SN54SC4T32-SEP
- SN54SC4T86-SEP