This user's guide is a quick reference to the features and options of the of the KDK350ADPTR-EVM. Topics include using the EVM, header pinout, backlight control, LCD interface control switches, and touchscreen interface.
SimpleLink, Code Composer Studio are trademarks of Texas Instruments.
Arm is a registered trademark of Arm Limited.
IAR Embedded Workbench is a registered trademark of IAR Systems.
All other trademarks are the property of their respective owners.
The KDK350ADPTR-EVM provides a physical adapter layer to interface the MSP432E411Y microcontroller (MCU) on the SimpleLink™ Ethernet MSP432E411Y MCU Evaluation Board (MSP432E411Y-BGAEVM) to a Kentec Display K350QVG-V2-F-04 LCD, including the LCD backlight driver. The KDK350ADPTR-EVM can be used as a reference for connecting other LCD modules to the MSP432E411Y-BGAEVM.
The Kentec Display K350QVG-V2-F-04 LCD is a 3.5-inch diagonal, 320-×240-pixel resolution, TFT module display that has LED backlighting and supports the i80 8-, 16-, or 18-bit interface and SPI. The display also includes an integrated resistive touch panel.
Figure 1 shows the KDK350ADPTR-EVM with key features highlighted.
The KDK350ADPTR-EVM is used with the MSP432E411Y-BGAEVM to showcase the 16-bit parallel LCD interface on the MSP432E411Y device. The SimpleLink MSP432E4 Software Development Kit (SDK) includes a graphics library example of the LCD capabilities of the MSP432E411Y MCU.
To use the KDK350ADPTR-EVM with an MSP432E411Y-BGAEVM and the graphics library example, follow these steps:
The KDK350ADPTR-EVM uses header J1 on the bottom of the EVM to connect to a microcontroller or LCD driver. Table 1 lists the pinout for J1. All of the signals are on the K350QVG LCD except for the backlight PWM signal on pin 32. Table 2 lists the connections between the LCD at J2 and J1.
Signal | J1 Pin | Signal | |
---|---|---|---|
3.3V | 1 | 2 | 5V |
DC | 3 | 4 | RESET |
RD | 5 | 6 | WR |
GND | 7 | 8 | CS |
8080_D1 | 9 | 10 | 8080_D2 |
8080_D3 | 11 | 12 | 8080_D4 |
8080_D5 | 13 | 14 | 8080_D6 |
8080_D7 | 15 | 16 | 8080_D8 |
8080_D10 | 17 | 18 | 8080_D11 |
8080_D12 | 19 | 20 | 8080_D13 |
8080_D14 | 21 | 22 | 8080_D15 |
8080_D16 | 23 | 24 | 8080_D17 |
NC | 25 | 26 | NC |
NC | 27 | 28 | NC |
NC | 29 | 30 | NC |
NC | 31 | 32 | Backlight PWM |
3.3V | 33 | 34 | 5V |
XL | 35 | 36 | XR |
YU | 37 | 38 | YD |
GND | 39 | 40 | GND |
J2 Pin | LCD Signal | J1 Pin | MSP432E411Y Signal |
---|---|---|---|
1 | Backlight LED Cathode | N/A | N/A |
2 | Backlight LED Cathode | N/A | N/A |
3 | Backlight LED Anode | N/A | N/A |
4 | Backlight LED Anode | N/A | N/A |
5 | GND | 7, 39, 40 | GND |
6 | XR | 36 | PP6 – AIN23 |
7 | YD | 38 | PE7 – AIN21 |
8 | XL | 35 | PP7 – AIN22 |
9 | YU | 37 | PE6 – AIN20 |
10 | GND | 7, 39,40 | GND |
11, 12 ,13 | No Connection | N/A | N/A |
14 | RESET | 4 | LCDMCLK |
15 | CS | 8 | LCDAC |
16 | SPCLK | 7, 39, 40 | GND |
17 | SDA-SDI | 7, 39, 40 | GND |
18, 19 | No Connection | N/A | N/A |
20 | D0 | 7, 39, 40 | GND |
21 | D1 | 9 | LCDDATA0 |
22 | D2 | 10 | LCDDATA1 |
23 | D3 | 11 | LCDDATA2 |
24 | D4 | 12 | LCDDATA3 |
25 | D5 | 13 | LCDDATA4 |
26, 27 | No Connection | N/A | N/A |
28 | D6 | 14 | LCDDATA5 |
29 | D7 | 15 | LCDDATA6 |
30 | D8 | 16 | LCDDATA7 |
31 | D9 | 7, 39, 40 | GND |
32 | D10 | 17 | LCDDATA8 |
33 | D11 | 18 | LCDDATA9 |
34, 35 | No Connection | N/A | N/A |
36 | D12 | 19 | LCDDATA10 |
37 | D13 | 20 | LCDDATA11 |
38 | D14 | 21 | LCDDATA12 |
39 | D15 | 22 | LCDDATA13 |
40 | D16 | 23 | LCDDATA14 |
41 | D17 | 24 | LCDDATA15 |
42 | HSYNC | 7, 39, 40 | GND |
43 | VSYNC | 7, 39, 40 | GND |
44 | DCLK | 7, 39, 40 | GND |
45, 46, 47, 48 | AVDD | 1, 33 | VDD |
49 | DC | 3 | LCDFP |
50 | RD | 5 | LCDCP |
51 | WR | 6 | LCDLP |
52, 53, 54, 55 | PS0, PS1, PS2, PS3 | N/A | N/A |
56 | WSYNC | N/A | N/A |
57 | No Connection | N/A | N/A |
58 | OE | 7, 39, 40 | GND |
59 | GND | 7, 39, 40 | GND |
60 | GND | 7, 39, 40 | GND |
The K350QVG-V2-F-04 LCD provides backlighting through six LEDs in a serial configuration which requires 19.2 V at 20 mA for full brightness. The backlight voltage is generated using a TI TPS61042 Switch Boost Converter. The TPS61042 allows PWM control over the backlight to adjust brightness using the Backlight PWM pin on J1 (pin 32). For full brightness, a logic "high" signal is applied to the Backlight PWM pin. For reduced brightness, a PWM signal between 100 Hz and 50 kHz is applied.
The K350QVG-V2-F-04 LCD supports for multiple interface modes:
The mode is selected by the PS3, PS2, PS1, and PS0 pins on the LCD. Table 3 lists the selection for each mode. Switch bank S1 on the KDK350ADPTR-EVM controls the PS3, PS2, PS1, and PS0 pins (see Figure 3). The silkscreen adjacent to S1 shows the signal that each switch controls and the position to generate a 1 or a 0. Figure 3 shows the switch configuration to use 8080 16-bit parallel interface.
PS3 | PS2 | PS1 | PS0 | Interface |
---|---|---|---|---|
0 | 0 | 1 | 0 | 16-bit 8080 parallel interface |
0 | 0 | 1 | 1 | 8-bit 8080 parallel interface |
0 | 1 | 0 | 0 | 9-bit RGB and 3-wire SPI |
0 | 1 | 0 | 1 | 16-bit RGB and 3-wire SPI |
0 | 1 | 1 | 0 | 18-bit RGB and 3-wire SPI |
0 | 1 | 1 | 1 | 6-bit RGB and 3-wire SPI |
1 | 0 | 1 | 0 | 18-bit 8080 parallel interface |
1 | 0 | 1 | 1 | 9-bit 8080 parallel interface |
1 | 1 | 1 | 0 | 3-wire SPI |
The SimpleLink MSP432E4 Software Development Kit (SDK) has examples and drivers for the KDK350ADPTR-EVM when used in conjunction with the MSP432E411Y-BGAEVM. The example projects draw to the LCD screen and use the touchscreen overlay. These examples are a starting point for the development of the final application for use on the MSP432E411Y-BGAEVM with KDK350ADPTR-EVM.
The source code is provided as part of the SimpleLink MSP432E4 SDK.
The source code installation includes directories containing projects, makefiles, and binaries for the following tool-chains:
For detailed information on using the tools, see the documentation included in the tool chain installation or visit the website of the tool supplier.
In compliance with the Article 33 provision of the EU REACH regulation, TI notifies you that this EVM includes components that contain at least one Substance of Very High Concern (SVHC) above 0.1%. These uses from Texas Instruments do not exceed 1 ton per year. Table 4 lists the SVHCs in this EVM.
Component Manufacturer | Component Part Number | SVHC Substance | SVHC CAS |
---|---|---|---|
Kentec Display | K350QVG-V2-F | 2-(2H-benzotriazol-2-yl)-4,6-ditertpentylphenol (UV-328) | 25973-55-1 |
Kentec Display | K350QVG-V2-F | Boric acid | 10043-35-3, 11113-50-1 |
Kentec Display | K350QVG-V2-F | Disodium tetraborate, anhydrous | 1303-96-4, 1330-43-4, 12179-04-03 |
Kentec Display | K350QVG-V2-F | Tetraboron disodium heptaoxide, hydrate | 12267-73-1 |
Kentec Display | K350QVG-V2-F | Diboron trioxide | 1303-86-2 |
Kentec Display | K350QVG-V2-F | Diarsenic pentaoxide | 1303-28-2 |