SLVUCE8A March   2022  â€“ February 2023 TPS7H5001-SP

 

  1.   Abstract
  2.   Trademarks
  3. 1TPS7H5001-SP WCA Model Specification
    1. 1.1 Parameter Variation
    2. 1.2 Global Variables
    3. 1.3 Editing Model Parameters
  4. 2Model Setup
    1. 2.1 Running Transient Simulation
    2. 2.2 Running POP Analysis and AC Simulation
  5. 3Monte Carlo
    1. 3.1 Monte Carlo Simulation
  6.   Revision History

Abstract

This user's guide is intended to define the Worst Case Analysis (WCA) PSpice model for the TPS7H5001-SP. Instructions on setting up the unencrypted model for simulationSIMPLIS® are also provided. The first section of the guide outlines the model parameters and development. The second section covers different options for setting the model up to run simulations. Finally, the third section addresses how to run different types of simulations.