The application report is a comprehensive technical manual to leverage the ROM bootloader to boot applications or secondary bootloaders on Keystone II devices like 66AK2H14 and 66AK2E05. This document provides boot examples along with description of boot utilities and setting up TI supported evaluation platforms to test the sample software.
Additionally, some of the frequently asked questions are addressed around this topic along with additional references to Processor SDK in the SDK documentation on ti.com to design your system boot.
The document is meant to be used as an addendum document to ARM Bootloader User Guide for KeyStone II Devices. The Processor SDK also provides secondary bootloaders that enable developers to enable two stage application booting, which allows for customization of the system boot beyond the capabilities of the ARM® ROM bootloader
Code Composer Studio is a registered trademark of Texas Instruments.
ARM is a registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
Linux is a registered trademark of Linus Torvalds in the U.S. and other countries.
All other trademarks are the property of their respective owners.