Ever since the introduction of the topology, phase-shifted full bridge rectifiers (PSFB) have gained a wide range of acceptance in industrial applications like power supplies, telecom rectifiers, battery charging systems, renewable energy systems, and so forth. Due to the ease of controllability, the PSFB rectifier is often selected as the go-to method for transferring bulk amounts of power from the high-voltage (HV) DC to the low-voltage (LV) DC side with electrical isolation. One such simple control scheme that can be used in this application is called peak current mode control (PCMC). The power transfer happens from the HV to LV side when the turn ON period of diagonally opposite switches of two legs overlap with each other. In PCMC, this overlapping period is controlled by making the appropriate peak current value setting. On top of this, an outer voltage control loop is implemented to maintain the output voltage at the desired level. In this work, the control mechanism is implemented using ARM R5F core-based SITARA MCU of Texas Instruments (TI) to showcase the real-time control capabilities. In addition to that, a synchronous rectification feature is implemented on the LV side to harness the optimized power output from the converter.