BCDMA |
i2431 — BCDMA: RX Channel can lockup in certain
scenarios |
YES |
Boot |
i2366 — Boot: ROM does not comprehend specific JEDEC SFDP features for
8D-8D-8D operation |
YES |
Boot |
i2371 — Boot: ROM code may hang in UART boot mode during data
transfer |
YES |
Boot |
i2410 — Boot: ROM may fail to boot due to i2409 |
YES |
Boot |
i2413 — Boot: HS-FS ROM boots corrupted ROM boot
image |
YES |
Boot |
i2414 — Boot: Ethernet PHY Scan and Bring-Up Flow
doesn't work with PHYs that don't support Auto Negotiation |
YES |
Boot |
i2417 — Boot: GPMC NAND configured to slower clock
speed |
YES |
Boot |
i2419 — Boot: When disabling deskew calibration, ROM
does not check if deskew calibration was enabled |
YES |
Boot |
i2420 — Boot: XSPI Boot time is not consistent in SFDP
mode |
YES |
Boot |
i2421 — Boot: fatTiny GPT handling causes data
abort |
YES |
Boot |
i2422 — Boot: ROM timeout for MMCSD filesystem boot
too long |
YES |
Boot |
i2423 — Boot: HS-FS ROM applies debug access
restrictions to all address space covered by the efuse controller
firewall |
YES |
Boot |
i2435 — Boot: ROM timeout for eMMC boot too
long |
YES |
c71x |
i2199 — C71x: SE returning incorrect data
when non-aligned transposed stream crosses AM1 circular buffer
boundary |
YES |
C7x |
i2120 — C71x: SE returning incorrect data when
non-aligned transposed stream crosses AM1 circular buffer
boundary |
YES |
C7x |
i2376 — C7x: SE/SA/HWAOPEN receives corrupted template
following two back to back VPUT/MVC instructions |
YES |
C7x |
i2399 — C7x: CPU NLC Module Not Clearing State on
Interrupt |
YES |
CPSW |
i2208 — CPSW: ALE IET Express Packet
Drops |
YES |
CPSW |
i2401 — CPSW: Host Timestamps Cause CPSW Port to Lock up |
YES |
ECC_AGGR |
i2049 —
ECC_AGGR: Potential IP Clockstop/Reset Sequence Hang due to Pending
ECC Aggregator Interrupts |
YES |
Interrupt
Aggregator |
i2196 —
IA: Potential deadlock scenarios in IA |
YES |
MCAN |
i2278 — MCAN: Message Transmit order not guaranteed from
dedicated Tx Buffers configured with same Message ID |
YES |
MCAN |
i2279 — MCAN: Specification Update for dedicated Tx
Buffers and Tx Queues configured with same Message ID |
YES |
MMCHS |
i2312 — MMCHS HS200 and SDR104 Command Timeout Window
Too Small |
YES |
OSPI |
i2189 —
OSPI: Controller PHY Tuning Algorithm |
YES |
OSPI |
i2249 — OSPI: Failing OSPI DDR PHY Internal Pad Loopback
and No Loopback timing modes |
YES |
OSPI |
i2383 — OSPI: 2-byte address is not supported in PHY
DDR mode |
YES |
PRG |
i2253 — PRG: CTRL_MMR STAT registers are unreliable indicators of POK
threshold failure |
YES |
PSIL |
i2137 — PSIL: Clock stop operation can result in
undefined behavior |
YES |
RAT |
i2062 —
RAT: Error Interrupt Triggered Even When Error Logging Disable Is
Set |
YES |
RESET |
i2407 — RESET: MCU_RESETSTATz unreliable when MCU_RESETz is asserted
low |
YES |
USART |
i2310 — USART: Erroneous triggering of timeout
interrupt |
YES |
USART |
i2311 — USART Spurious DMA
Interrupts |
YES |
USB |
i2134 — USB: 2.0 Compliance Receive
Sensitivity Test Limitation |
YES |
USB |
i2409 — USB: USB2 PHY locks up due to short suspend |
YES |