Richard Zarr
When building analog signal chains for precision, you should consider several factors during component selection to maintain accuracy in your resulting measurements: offset, offset drift (with temperature), gain error or linearity, and low-frequency noise. In many high-precision applications, the source signal is very small and requires a great deal of gain to adjust the signal level. This is very common in precision data-acquisition systems, where you must adjust the source signal to match the input range of an analog-to-digital converter (ADC).
At first glance, you might select a typical operational amplifier, not realizing that the offset voltage is input referred – and thus affected by gain. When you add a significant amount of gain such as A=100, the offset voltage may add significant error. For example, if you have a typical amplifier with an input offset of 3mV and a gain of 100, you have a potential full-scale error of 300mV, or roughly one-third of a volt. For a 3.3V input ADC, the system would have an error of roughly 10%.
Over the years, designers have made great strides in precision amplifier design to remove offset and calibrate it over temperature, resulting in excellent drift numbers. But with improved precision, other factors begin to dominate – mostly driven by amplifier architecture or physics and lumped together in the category of “noise,” or electrical uncertainty.
A group of precision amplifiers called chopper-stabilized amplifiers use an alternative switched path to null the input offset. This technique does an excellent job of removing offset and tracking with temperature, but can also introduce chopping noise. The noise tends to be above 10kHz, however, so you can easily filter it out of most precision applications where the time constant is fairly long (such as when measuring temperature).
There is another insidious noise source called 1/f (one-over-f) noise, also known as flicker noise. As the name implies, flicker noise increases with decreasing frequency – typically in the region of low-frequency precision measurements. The noise power has an average slope of -10db/decade and is caused by various physical properties of the amplifier’s semiconductor material (see Figure 1). The 1/f noise is unbounded and increases with time, making the measurement of this noise source very difficult – unless you want to wait years to get your answer. This noise source dominates at low frequency, and like my earlier input-offset example, is also a function of gain. So in high-gain systems (A > 100), this noise can be significant.
In an effort to combat this noise source, a new class of devices has arrived that has solved the 1/f noise issue. The INA188 is an instrumentation amplifier that not only has exceptional world-class offset and drift specifications, but eliminates the 1/f corner where the flicker noise intersects the wideband noise, providing a flat noise floor down to 0.1Hz. This can help improve applications such as strain gauges that use bridge topologies or other high-precision measurements used in process control. These types of measurements typically use very high levels of gain and suffer from the increased low-frequency flicker noise found in most precision amplifiers.
If you want to know more about 1/f noise and its implications, check out this excellent blog post, which includes the Excel spreadsheet used to create Figure 1.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated