DESIGN GUIDE
Grid Connected Inverter Reference Design
Revision History
Changes from C Revision (May 2019) to D Revision
- Changed powerSUITE Page for the Grid Connected Inverter Solution imageGo
- Changed Project Explorer View of Solution Project imageGo
- Changed Current Loop Design Using Compensation Designer imageGo
- Changed Compensation Designer With Measured Plant Frequency Response Data imageGo
- Changed SPRUHZ5 to SPRUIK4 linkGo
Changes from B Revision (November 2017) to C Revision
- Changed TMS310F280049M to TMS310F280049CGo
- Added and TMS320F280049CGo
- Changed TMS310F280049M from block diagram to TMS320F280049CGo
- Deleted TMS310F280049M from block diagramGo
- Changed TMS320F280049M to TMS320F280049CGo
- Changed <sdk_install_path>\c2000ware\boards\controlcards\TMDSCNCD280049M to <sdk_install_path>\c2000ware\boards\controlcards\TMDSCNCD280049CGo
- Changed TMS320F280049M to TMS320F280049CGo
- Changed TMS320F280049M to TMS320F280049CGo
Changes from A Revision (October 2016) to B Revision
- Updated formatting to fit current design guide templateGo
- Added TMS320F280049M to ResourcesGo
- Added "Supports TMS320F28377D and TMS320F280049M" to FeaturesGo
- Added TMS320F280049M to the block diagramGo
- Changed location of Excel sheet of calculationsGo
- Changed location of info sheet in Section 3.1.1.2: Control Card SettingsGo
- Added required settings for revision A of the TMS320F280049M control card in Section 3.1.1.2: Control Card SettingsGo
- Added note in Section 3.1.2: Firmware: powerSUITE and Incremental Build SoftwareGo
- Changed Step 5 in Section 3.1.2.1: Opening the Project Inside Code Composer Studio™Go
- Updated Figure 21: Build Level 1 Control Diagram: Open Loop ProjectGo
- Changed 1.26 VRMS to 1.26 IRMS in Step 13 in Section 3.1.2.3.1.5: Running the CodeGo
- Updated Figure 26: Build Level 2 Control Diagram: Closed Current LoopGo
- Changed location of the SFRA.exe file from controlSUITE/libs/app_libs/SFRA/<version>/GUI to <sdk_install_path>/libraries/sfra/GUIGo
- Changed invloRefInst to invIoRef in Step 46 in Section 3.1.2.3.2.4: Running the CodeGo
- Deleted the step "Set the clearInvTrip variable to 1 to clear the inverter trip" in Section 3.1.2.3.3.2: Running the CodeGo
- Added the TMS320F28004x Piccolo™ Microcontrollers Technical Reference Manual to Section 6: Related DocumentationGo
- Added the TMS320F28004x Piccolo™ Microcontrollers Data Sheet to Section 6: Related DocumentationGo
Changes from * Revision (November 2015) to A Revision
- Added TIEVM-HV-1PH-DCAC product page link in Design ResourcesGo
- Added configuration (CFG)Go
- Added Figure 12: Control Scheme Used for Grid Connected Inverter ControlGo
- Added note in Section 3: Getting Started With HardwareGo
- Deleted "Keep in mind that the output capacitor is large (for example, 20 uF)." from Step 2 in Section 3.1: Base Board SettingsGo
- Changed the control card slot from H5 to J15-J16Go
- Changed isolated HV DC source connection from CON1 to J17Go
- Changed Figure 16: Hardware Setup to Run Software for BUILD Level 1Go
- Added Section 3.3: Tips to Connect JTAG USB CableGo
- Added Section 4.1.2: Open TI Design Software for AdaptationGo
- Added "up to 50 V" to Step 9 under Running the CodeGo
- Added "Now raise the DC Bus voltage slowly up to 380 V" to Step 10 under Running the CodeGo
- Deleted "Check the frequency of the generated AC waveform." from Running the CodeGo
- Deleted "Confirm that the generated AC waveform matches the value entered on the powerSUITE page (for example, 60 Hz)." from Running the CodeGo
- Changed variable from sine_mains.SigFreq to guiFreqAvgGo
- Changed output voltage from 133 VRMS to 126 VRMSGo
- Changed current from 1.35 VRMS to 1.26 VRMSGo
- Changed numeration after Figure 25: BUILD LEVEL 1 Graph1.GraphProp File Showing Measured Per-Unit Voltage and Current ValuesGo
- Added Figure 27: Hardware Setup to Run Software for Build Level 2: DC CheckGo
- Deleted "Turn the S1 switch to the ON position."Go
- Added note under Running the CodeGo
- Changed title in Figure 32 from "Setup for DC Check of the Current Controller" to "Hardware Setup to Run Software for BUILD Level 2: AC Check"Go
- Added note after Step 8 in Running the CodeGo
- Changed Steps 2 through 9 under Running the CodeGo
- Deleted Steps 10 through 13 under Running the CodeGo
- Changed Step 16 under Running the CodeGo