EMBEDDED-PROGRAMMING

EMBEDDED-PROGRAMMING

Downloads

Overview

Each product that has an embedded CC3120/CC3220 device on board must also have a serial flash device connected. The serial flash must be formatted and, at minimum, be programmed with the Service Pack that contains necessary software updates and additional features. In the case of CC3220, a binary image running on the internal MCU processor must also be programmed. There are several existing options for serial flash programming:

  • Uniflash – A PC based utility offering Image creation and programming. Content is programmed via UART.
  • Over The Air programming – Content is delivered through a network connection. However, this requires the serial flash to be formatted in advance during production. Content is programmed via the host interface (UART or SPI).
  • Industrial Flash Programming – flashing a complete image prepared with Uniflash directly to the serial flash. Can be applied when no simplelink device is attached to the serial flash. Content is programmed via the serial flash SPI lines.

The new Embedded Programming is an additional option that leverages the programming feature of Uniflash, but eliminates the need of a PC. Image Programming tool and source code can be leveraged by customers and used as a reference to implement their own PC tool, program an external programmer on production line, or embed it into their product. The primary use of this tool is for some production line setups that may not have a connected PC, but an embedded device (e.g. MCU, FPGA, DSP, etc) for programming instead. Note that this tool is not a replacement for Uniflash. Some key feature differences includes:

  • Uniflash has more functionalities that just image programming
  • The embedded programming implements just a subset of options exposed in boot loader. Uniflash uses all.
  • An image needs to be prepared before applying Embedded Programming, and this image can only be created with Uniflash.
  • The source code of this Embedded Programming is provided for custom implementation.
Download View video with transcript Video

Downloads

Software programming tool

CC3X00EMBEDDEDPROG Embedded Programming for CC3100 & CC3200

Supported products & hardware

CC3X00EMBEDDEDPROG Embedded Programming for CC3100 & CC3200

close
Latest version
Version: null
Release date: Aug 23, 2024
Software programming tool

CC3X20EMBEDDEDPROG Embedded Programming for CC3120 & CC3220

Supported products & hardware

CC3X20EMBEDDEDPROG Embedded Programming for CC3120 & CC3220

close
Latest version
Version: null
Release date: Aug 23, 2024

Technical documentation

No results found. Please clear your search and try again.
View all 1
Top documentation Type Title Format options Date
User guide CC3120 and CC3220 Simplelink™ Wi-Fi® Embedded Programming User's Guide (Rev. A) PDF | HTML Jun 29, 2018

Related design resources

Software development

SOFTWARE DEVELOPMENT KIT (SDK)
CC3100SDK SimpleLink Wi-Fi CC3100 Software Development Kit (SDK) CC3200SDK SimpleLink Wi-Fi CC3200 Software Development Kit (SDK) SIMPLELINK-WIFI-CC3120-SDK-PLUGIN SIMPLELINK-SDK-WIFI-PLUGIN
SOFTWARE PROGRAMMING TOOL
UNIFLASH UniFlash flash programming tool

Hardware development

DEVELOPMENT KIT
CC3120BOOST SimpleLink™ Wi-Fi® CC3120 wireless network processor BoosterPack™ plug-in module CC3220S-LAUNCHXL CC3220S LaunchPad™ development kit for Wi-Fi® SimpleLink™ wireless MCU CC3220SF-LAUNCHXL CC3220SF LaunchPad™ development kit for Wi-Fi® SimpleLink™ wireless MCU
EVALUATION BOARD
CC3100BOOST SimpleLink™ Wi-Fi® CC3100 wireless network processor BoosterPack™ plug-in module CC31XXEMUBOOST Advanced emulation kit for SimpleLink™ Wi-Fi® CC31xx BoosterPack™ plug-in module CC3200-LAUNCHXL SimpleLink Wi-Fi CC3200 LaunchPad

Support & training

TI E2E™ forums with technical support from TI engineers

View all forum topics

Content is provided "as is" by TI and community contributors and does not constitute TI specifications. See terms of use.

If you have questions about quality, packaging or ordering TI products, see TI support.

Videos