SLVAFE0 February 2023 TPS62441-Q1 , TPS62442-Q1 , TPS62810-Q1 , TPS62811-Q1 , TPS62812-Q1 , TPS62813-Q1 , TPS628501-Q1 , TPS628502-Q1 , TPS628503-Q1 , TPS62870 , TPS62870-Q1 , TPS62871 , TPS62871-Q1 , TPS62872 , TPS62872-Q1 , TPS62873 , TPS62873-Q1 , TPS62874-Q1 , TPS62875-Q1 , TPS62876-Q1 , TPS62877-Q1 , TPSM8287A06 , TPSM8287A10 , TPSM8287A12 , TPSM8287A15
The efficient design of a power delivery network PDN is a challenging task because all the segments of PDN are linked with each other. Changes in one component can have a significant influence on all the other components. This application note focuses on designing of filters and also discusses the stability problems caused by adding the input filter or the second stage of output LC filter if they are not designed properly by keeping a look on certain important parameters. Furthermore, the application note also explains the damping methods for resolving the stability issues caused by the addition of filters with step-down converter.