BQEVSW — bq Evaluation Software (bqEVSW) v0.0.92 for bq30z554-R1
支持的产品和硬件
产品
电池电量监测
BQEVSW — bq Evaluation Software (bqEVSW) v0.0.92 for bq30z554-R1
bqEVSW 0.09.0092 windows installer
bq 评估软件 (bqEVSW) 作为一种软件工具,可帮助您评估、配置、测试 bq20xxx 和 bq30xxx 系列 TI 电池管理产品以及利用其进行设计或以其他方式对其加以利用。它包含的功能可提供对寄存器和数据存储器的完全访问,其中包括对实时记录、直接低层通信的支持以及对配置和校准的支持。
有关 EV2300 的注意事项:EV2300 产品页面提供了用于 32 位 Windows 的驱动程序。TI e2e 论坛上发布了非官方 64 位 EV2300 驱动程序,也许可用于 64 位 Windows 7 或更高版本的 64 位 Windows。
** 可能需要安装 EV2400 产品页面上的 EV2400 支持组件。
bqEVSW 0.09.0092 windows installer
SDK, API, and Programmer installer
Quick Tips text document for Command line programmers
Software Manifest
Description:
BQ-BATTERY-PROGRAMMER-SW software development kit (SDK) is a collection of robust software command line tools that assist with the process of programming, testing, or assembling packs that use TI Battery management products. The executables in this software work with the MKST-3P-ALT-EV2300 MKS Technology alternative for EV2300 communications transceiver. The executables work with a single station but can be extended to multiple stations by using additional software and GUI from MKS Technology Inc. . Support for multiple stations is not included in this software.
There are multiple executables in the download, usually one per family of products. Older products such as BQ20xxx and BQ30xxx are also supported. Examples using the C++ programming language API and Python® programming language are provided for custom development.
Requirements:
Features:
Getting started:
1. Download the software
2. Run the installer
3. The executables, C API and Python API files can be found in the install location
4. Run the command line executable without arguments to get usage help. Refer to Readme.txt in the install folder for more information and how to get help using the command line.
Software installer to enable BQEVSW to use MKST-3P-ALT-EV2300
Software manifest
Description:
BQEVSW-MKST-UPDATE software is a software update for BQEVSW (bq Evaluation Software) and BQEASY (bq EV-Easy) to allow it to work with the MKST-3P-ALT-EV2300 MKS Technology alternative for EV2300 communications transceiver. This update installs a program that allows switching the USB transceiver target in software like BQEVSW and BQEASY from/to EV2300 to/from MKST-3P-ALT-EV2300.
The program requires administrator privileges.
Requirements:
Features:
Getting started:
1. Download the software
2. Run the installer and check the option to create shortcuts
3. Run the program using shortcut named BQEVSW-MKST-UPDATE from Start menu/Desktop
4. Allow administrator privilege when/if prompted
5. On the GUI window that opens, select the target transceiver to support and follow steps to switch
6. Connect matching transceiver and start BQEVSW, BQEASY or other similar software.
Note: BQMTESTER-MKST-UPDATE and BQEVSW-MKST-UPDATE both update the same software components. Switching the USB transceiver using any of these shortcuts will also switch it in the other.
Important Note: The latest chemistry updater for bqStudio requires bqStudio 1.3.86 or higher. |
Instructions for bqStudio Chemistry database update:
Instructions for bqEVSW Chemistry database update: