驱动程序或库
SPRC223
C672x 芯片支持库 (CSL)
SPRC223
概述
The Chip Support Library (CSL) provides an application programming interface (API) used for configuring and controlling the DSP on-chip peripherals for ease of use and hardware abstraction. This will shorten development time by providing standardization and portability. The functions listed in the features section are specifically designed for C672x devices.
特性
The release is provided as three sets of zip files.
- The product zip file csl_C672x_v3_00_08_04.zip contains the following files:
- CSL header files
- CSL libraries
- CSL example projects and source files
- CSL Reference Guide
- The interrupt controller (INTC) zip file csl_C672x_intc_v3_00_08_04.zip contains the following files:
- INTC header files
- INTC library
- INTC example project and source files
- The source zip file csl_C672x_src_v3_00_08_04.zip contains the following files:
- CSL header files
- CSL source files
- Makefile and batch files
下载
技术文档
未找到结果。请清除搜索,并重试。
查看全部 1
类型 | 标题 | 下载最新的英语版本 | 日期 | |||
---|---|---|---|---|---|---|
应用手册 | Migrating from CSL 2.x to CSL 3.x | 2006年 1月 26日 |