选择版本
SIMPLELINK-BLE-PLUGIN-AZURE-GATEWAY-EXAMPLE-PACK
SimpleLink™ Bluetooth low energy plug-in Azure™ gateway example pack
Windows Installer for SimpleLink BLE Plug-in Azure Gateway Example Pack
macOS Installer for SimpleLink BLE Plug-in Azure Gateway Example Pack
Linux Installer for SimpleLink BLE Plug-in Azure Gateway Example Pack
产品
Arm Cortex-M4 MCU
低功耗 2.4GHz 产品
硬件开发
开发套件
评估板
文档
SimpleLink BLE Plug-in Azure Gateway Example Pack User's Guide
发布信息
The SimpleLink SDK BLE Plugin Azure Gateway Example Pack is a companion software packages that enables a user to enable their BLE applications as a gateway to the Azure Cloud.
This Examples Pack requires prior download of the SimpleLink SDK BLE Plugin, as well as the SimpleLink SDK E4 Azure Plugin. Without prior installation of those plugins, as well as their SDK dependencies, the examples in this Example Pack will not work.
新增功能
- First release of the SimpleLink BLE Plugin Azure Gateway Example Pack.
- This release contains the azure_gateway example, which demonstrates how a 2-chip GAP central role solution can act as a gateway to the Azure IoT cloud. This feature uses the MSP432E401Y as the Host device and the CC26x2R1 as the NWP. The source code used for this example can be found in the SimpleLink Bluetooth Plugin and in the SimpleLink MSP432E4 SDK Azure IoT Plugin. The azure_gateway example demonstrates the following features:
- Host: MSP432E401Y
- NWP: CC26X2R1
- GAP Central role support
- Host Controller Interface (HCI) protocol used for communication with the NWP
- BLE5 support
- Power management
- Low Energy Secure Connection (LESC) Pairing
- Tested with up to 4 peripherals connected simultaneously (but can support more than 4 connections)
- Supports a subset of TI Vendor Specific HCI commands and Bluetooth LE HCI commands/events. More information on these APIs can be found BLE Vendor Specific API Guide.
- Works out-of-box with the Sensors BoosterPack and Project Zero examples that are also in the SimpleLink SDK Bluetooth Plugin.