CC1111EMK868-915

CC1111 USB 评估模块套件 868/915 MHz

CC1111EMK868-915

立即订购

概述

The CC1111 USB dongle makes it easy to have a direct connection between a PC and a sub-1 GHz network based on compatible radios, like the CC1101, CC1120, CC1110, and CC430. The dongle is a complete reference design demonstrating how to use the USB and RF interfaces on the CC1111 system-on-chip.

The dongle operates in the 868 MHz and 915 MHz frequency bands.

  • Use the USB firmware and examples (swrc088) as a basis to develop and test USB device software for the CC1111. If you have the complete CC1110-CC1110DK, you can run several examples:
    • Wireless serial port application (CDC)
    • Wireless mouse and keyboard (HID)
    • Any other USB class can also be implemented based on the generic USB firmware library. Refer to the USB firmware user guide for more information.
  • Use the dongle as a packet capture device for the SmartRF Packet Sniffer. Configured correctly, the dongle can capture packets over-the-air and the sniffer application can parse and display the contents.

Note that a SmartRF04EB (included in the CC1110-CC1111DK) or a CC-Debugger (sold separately) is needed to program the CC1111 device.

Also note that the CC1111 USB Dongle has passed USB compliance tests. The USB TID is 10005584.

特性

The CC1111 USB Evaluation Kit includes:

  • One CC1111 USB dongle with chip antenna for 868 and 915 MHz operation

下载 观看带字幕的视频 视频

立即订购并开发

子卡

CC1111EMK868-915 — CC1111EMK868-915 评估模块套件

登录以订购
In stock / Out of stock
数量限制:
TI.com 上无现货
固件

SWRC088 — CC USB Firmware Library and Examples

支持的产品和硬件
下载

SWRC088 CC USB Firmware Library and Examples

close
最新版本
版本: 01.00.00.0C
发布日期: 30 十一月 2009

校验和
产品
低功耗 2.4GHz 产品
CC2531 具有高达 256kB 闪存和 8kB RAM 的 Zigbee 和 IEEE 802.15.4 无线 MCU
Sub-1GHz 无线 MCU
CC1110-CC1111 具有高达 32kB 闪存的低于 1GHz 无线 MCU
其他无线产品
CC2510 2.4GHz 无线电收发器、8051 MCU 和 16KB 或 32KB 存储器 CC2511 2.4GHz 无线电收发器、8051 MCU、16KB 或 32KB 闪存和全速 USB 接口 CC2511F8 2.4GHz 无线电收发器、8051 MCU、8KB 闪存和全速 USB 接口 CC2531-RF4CE 具有高达 256kB 闪存和 8kB RAM 的 Zigbee、IEEE 802.15.4 和 RF4CE 无线 MCU
硬件开发
子卡
CC1111EMK868-915 CC1111 USB 评估模块套件 868/915 MHz CC2531EMK CC2531 USB 评估模块套件

发布信息

The design resource accessed as www.ti.com.cn/lit/zip/swrc088 or www.ti.com.cn/lit/xx/swrc088c/swrc088c.zip has been migrated to a new user experience at www.ti.com.cn/tool/cn/download/SWRC088. Please update any bookmarks accordingly.
应遵守 TI 的评估模块标准条款与条件.

技术文档

未找到结果。请清除搜索,并重试。
查看所有 4
类型 标题 下载最新的英文版本 日期
证书 CC1111EMK868-915 EU Declaration of Conformity (DoC) 2019年 1月 2日
用户指南 CC1111 USB Evaluation Module Kit 868/915 MHz Quick Start Guide 2015年 11月 5日
用户指南 CC1111/CC2511 USB HW User's Guide (Rev. B) 2009年 7月 31日
用户指南 CC USB Software Examples User's Guide 2009年 5月 11日

相关设计资源

软件开发

驱动程序或库
SIMPLICITI 符合 SimpliciTI 的协议堆栈

设计工具和仿真

计算工具
PACKET-SNIFFER SmartRF 协议软件包监听器

支持与培训

可获得 TI E2E™ 论坛的工程师技术支持

查看所有论坛主题 查看英文版所有论坛主题

所有内容均由 TI 和社区网友按“原样”提供,并不构成 TI 规范。参阅使用条款

如果您对质量、包装或订购 TI 产品有疑问,请参阅 TI 支持

视频