选择版本

选择版本

未找到结果。请清除搜索并重试。

SIMPLELINK-SDK-TI-15-4-STACK-PLUGIN

适用于 SimpleLink™ MCU SDK 的 TI 15.4 Stack 插件

选择版本
未找到结果。请清除搜索并重试。
最新版本
版本: 2.20.00.05
发布日期: 2018-6-28

Windows Installer for SimpleLink SDK TI 15.4 Stack Plugin

MD5 校验和

macOS Installer for SimpleLink SDK TI 15.4 Stack Plugin

MD5 校验和

Linux Installer for SimpleLink SDK TI 15.4 Stack Plugin

MD5 校验和
lock = 需要出口许可(1 分钟)
产品
Arm Cortex-M4 MCU
MSP432E401Y 具有以太网、CAN、1MB 闪存和 256kB RAM 的 SimpleLink™ 32 位 Arm Cortex-M4F MCU
Sub-1GHz 无线 MCU
CC1310 具有 128kB 闪存的 SimpleLink™ 32 位 Arm Cortex-M3 低于 1GHz 无线 MCU CC1350 具有 128kB 闪存的 SimpleLink™ 32 位 Arm Cortex-M3 多协议低于 1GHz 和 2.4GHz 无线 MCU
Wi-Fi 产品
CC3220R 具有 6 个 TLS/SSL 插槽和 256kB RAM 的 SimpleLink™ 32 位 Arm Cortex-M4 Wi-Fi® 无线 MCU CC3220S 具有安全启动和 256kB RAM 的 SimpleLink™ 32 位 Arm Cortex-M4 Wi-Fi® 无线 MCU CC3220SF 具有 1MB 闪存和 256kB RAM 的 SimpleLink™ 32 位 Arm Cortex-M4 Wi-Fi® 无线 MCU
硬件开发
开发套件
CC3220S-LAUNCHXL CC3220S LaunchPad™ development kit for Wi-Fi® SimpleLink™ wireless MCU CC3220SF-LAUNCHXL CC3220SF LaunchPad™ development kit for Wi-Fi® SimpleLink™ wireless MCU LAUNCHXL-CC1350 CC1350 LaunchPad™ development kit for SimpleLink™ dual-band wireless MCU MSP-EXP432E401Y MSP432E401Y LaunchPad™ development kit for Ethernet SimpleLink™ MCU
评估板
LAUNCHXL-CC1310 CC1310 LaunchPad™ development kit for sub-1-GHz SimpleLink™ wireless MCU

文档

SimpleLink SDK TI 15.4 Stack Plugin Users Guide

发布信息

The SimpleLink™ SDK TI 15.4 Stack Plug-in is a companion software package that enables the use of the IEEE 802.11.15.4 stack from TI on any standard SimpleLink microcontroller (MCU). This plug-in supports the SimpleLink Sub-1 GHz CC1310 wireless MCU as a network processor. This software package works in tandem with the SimpleLink MSP432™ software development kit (SDK) or the SimpleLink Wi-Fi® CC3220 SDK to provide a portable implementation of the TI 15.4 Stack. By being able to seamlessly and modularly add TI 15.4 stack functionality to an embedded system, a developer can enable their embedded device to become a gateway to various IoT infrastructures.

新增功能

Added TI 15.4 Gateway to IBM code example that demonstrates how to implement a Personal Area Network (PAN) Coordinator device that sends incoming data from a sensor device to the IBM Watson IoT service. Improved debug statements in the code examples. Updated version number to match that of latest validated SDK (instead of 1.70.00.xx this release is 2.20.00.xx as we are testing against the 2.20.00.xx versions of the SDK)