The TPD8S300 is a single chip USB Type-C port protection solution that provides 20-V
Short-to-VBUS overvoltage and IEC ESD protection.
Since the release of the USB Type-C connector, many products and accessories for USB
Type-C have been released which do not meet the USB Type-C specification. One example of this is
USB Type-C Power Delivery adaptors that only place 20 V on the VBUS line.
Another concern for USB Type-C is that mechanical twisting and sliding of the connector could short
pins due to the close proximity they have in this small connector. This can cause 20-V
VBUS to be shorted to the CC and SBU pins. Also, due to the close proximity
of the pins in the Type-C connector, there is a heightened concern that debris and moisture will
cause the 20-V VBUS pin to be shorted to the CC and SBU pins.
These non-ideal equipments and mechanical events make it necessary for the CC and SBU
pins to be 20-V tolerant, even though they only operate at 5 V or lower. The TPD8S300 enables the
CC and SBU pins to be 20-V tolerant without interfering with normal operation by providing
overvoltage protection on the CC and SBU pins. The device places high voltage FETs in series on the
SBU and CC lines. When a voltage above the OVP threshold is detected on these lines, the high
voltage switches are opened up, isolating the rest of the system from the high voltage condition
present on the connector.
Finally, most systems require IEC 61000-4-2 system level ESD protection for their
external pins. The TPD8S300 integrates IEC 61000-4-2 ESD protection for the CC1, CC2, SBU1, SBU2,
DP_T (Top side D+), DM_T (Top Side D–), DP_B (Bottom Side D+), DM_B (Bottom Side D–) pins, removing
the need to place high voltage TVS diodes externally on the connector.
The TPD8S300 is a single chip USB Type-C port protection solution that provides 20-V
Short-to-VBUS overvoltage and IEC ESD protection.
Since the release of the USB Type-C connector, many products and accessories for USB
Type-C have been released which do not meet the USB Type-C specification. One example of this is
USB Type-C Power Delivery adaptors that only place 20 V on the VBUS line.
Another concern for USB Type-C is that mechanical twisting and sliding of the connector could short
pins due to the close proximity they have in this small connector. This can cause 20-V
VBUS to be shorted to the CC and SBU pins. Also, due to the close proximity
of the pins in the Type-C connector, there is a heightened concern that debris and moisture will
cause the 20-V VBUS pin to be shorted to the CC and SBU pins.
These non-ideal equipments and mechanical events make it necessary for the CC and SBU
pins to be 20-V tolerant, even though they only operate at 5 V or lower. The TPD8S300 enables the
CC and SBU pins to be 20-V tolerant without interfering with normal operation by providing
overvoltage protection on the CC and SBU pins. The device places high voltage FETs in series on the
SBU and CC lines. When a voltage above the OVP threshold is detected on these lines, the high
voltage switches are opened up, isolating the rest of the system from the high voltage condition
present on the connector.
Finally, most systems require IEC 61000-4-2 system level ESD protection for their
external pins. The TPD8S300 integrates IEC 61000-4-2 ESD protection for the CC1, CC2, SBU1, SBU2,
DP_T (Top side D+), DM_T (Top Side D–), DP_B (Bottom Side D+), DM_B (Bottom Side D–) pins, removing
the need to place high voltage TVS diodes externally on the connector.