CD4059A
- Synchronous Programmable
N Counter:
N = 3 to 9999 or 15,999 - Presettable down-counter
- Fully static operation
- Mode-select control of initial decade counting function (
10,8,5,4,2)
- T2L drive capability
- Master preset initialization
- Latchable
N output
- Quiescent current specified to 15 volts
- Max. input leakage current of 1 µA at 15 volts, full package-temperature range
- 1 volt noise margin, full package-temperature range
- 5-V and 10-V parametric ratings
- Applications
- Communications digital frequency synthesizers: VHF, UHF, FM, AM, etc.
- Fixed or programmable frequency division
- "Time out" timer for consumer-application industrial controls
- Companion Application Note, ICAN-6374, "Application of the CMOS CD4059A Programmable Divide-by-N Counter in FM and Citizens Band Transceiver Digital Tuners"
Data sheet acquired from Harris Semiconductor.
CD4059 standard "A" Series types are divide-by-N down-counters that can be programmed to divide an input frequency by any number "N" from 3 to 15,999. The output signal is a pulse one clock-cycle wide occurring at a rate equal to the input frequency divided by N. This single output has TTL drive capability. The down-counter is preset by means of 16 jam inputs.
The three Mode-Select Inputs Ka, Kb, and Kc determine the modulus ("divide-by" number) of the first and last counting
sections in accordance with the truth table shown in Table 1. Every time the first (fastest) counting section goes through
one cycle, it reduces by 1 the number that has been preset (jammed) into the three decades of the intermediate counting
section and into the last counting section, which consists of flip-flops that are not needed for operating the first counting
section. For example, in the 2 mode, only one flip-flop is needed in the first counting
section. Therefore the last counting section has three flip-flops that can be preset to a maximum count of seven with a place
value of thousands. If
10 is desired for the first section, Ka is set 1, Kb to 1, and Kc
to 0. Jam Inputs J1, J2, J3, and J4 are used to preset the first counting section and there is no last counting section. The
intermediate counting section consists of three cascaded BCD decade (
10) counters
presettable by means of Jam Inputs J5 through J16.
The Mode-Select Inputs permit frequency-synthesizer channel separations of 10, 12.5, 20, 25, or 50 parts. These inputs set the maximum value of N at 9999 (when the first counting section divides by 5 or 10) or 15,999 (when the first counting section divides by 8, 4, or 2).
The three decades of the intermediate counting section can be preset to a binary 15 instead of a binary 9, while their
place values are still 1, 10, and 100, multiplied by the number of the N mode. For
example in the
8 mode, the number from which counting-down begins can be preset to:
- 3rd decade: 1500
- 2nd decade: 150
- 1st decade: 15
- Last counting section 1000
The total of these numbers (2665) times 8 equals 21,320. The first counting section can be preset to 7. Therefore,
21,327 is the maximum possible count in the 8 mode.
The highest count of the various modes is shown in the column entitled Extended Counter Range of Table 1. Control inputs Kb and Kc can be used to initiate and lock the counter in the "master preset" state. In this condition the flip-flops in the counter are preset in accordance with the jam inputs and the counter remains in that state as long as Kb and Kc both remain low. The counter begins to count down from the preset state when a counting mode other than the master preset mode is selected.
The counter should always be put in the master preset mode before the 5 mode is selected.
Whenever the master preset mode is used, control signals Kb=0 and Kc=0 must be applied for at least 3 full clock pulses.
After the Master Preset Mode inputs have been changed to one of the modes, the next
positive-going clock transition changes an internal flip-flop so that the countdown can begin at the second positive-going
clock transition. Thus, after an MP (Master Preset) mode, there is always one extra count before the output goes high.
Fig. 1 illustrates a total count of 3 (
8 mode). If the Master Preset mode is started
two clock cycles or less before an output pulse, the output pulse will appear at the time due. If the Master Preset Mode
is not used the counter jumps back to the "JAM" count when the output pulse appears.
A "1" on the Latch Enable input will cause the counter output to remain high once an output pulse occurs, and to remain in the high state until the latch input returns to "0". If the Latch Enable is "0", the output pulse will remain high for only 1 cycle of the clock-input signal.
As illustrated in the sample applications, this device is particularly advantageous in communication digital frequency synthesis (VHF, UHF, FM, AM, etc.) where programmable divide-by-"N" counters are an integral part of the synthesizer phase-locked-loop sub-system. The CD4059A can also be used to perform the synthesizer "Fixed Divide-by-R" counting function. It is also useful in general-purpose counters for instrumentation functions such as totalizers, production counters, and "time out" timers.
The CD4059B-series types are supplied in 24-lead dual-in-line plastic packages (E suffix), and 24-lead small-outline packages (M and M96 suffixes).
您可能感兴趣的相似产品
功能与比较器件相似
技术文档
类型 | 标题 | 下载最新的英语版本 | 日期 | |||
---|---|---|---|---|---|---|
* | 数据表 | CD4059A TYPES 数据表 (Rev. B) | 2003年 6月 20日 | |||
选择指南 | Logic Guide (Rev. AB) | 2017年 6月 12日 | ||||
应用手册 | Understanding and Interpreting Standard-Logic Data Sheets (Rev. C) | 2015年 12月 2日 | ||||
选择指南 | 逻辑器件指南 2014 (Rev. AA) | 最新英语版本 (Rev.AB) | 2014年 11月 17日 | |||
用户指南 | LOGIC Pocket Data Book (Rev. B) | 2007年 1月 16日 | ||||
应用手册 | Semiconductor Packing Material Electrostatic Discharge (ESD) Protection | 2004年 7月 8日 | ||||
用户指南 | Signal Switch Data Book (Rev. A) | 2003年 11月 14日 | ||||
应用手册 | Understanding Buffered and Unbuffered CD4xxxB Series Device Characteristics | 2001年 12月 3日 |
设计和开发
如需其他信息或资源,请点击以下任一标题进入详情页面查看(如有)。
14-24-LOGIC-EVM — 采用 14 引脚至 24 引脚 D、DB、DGV、DW、DYY、NS 和 PW 封装的逻辑产品通用评估模块
14-24-LOGIC-EVM 评估模块 (EVM) 设计用于支持采用 14 引脚至 24 引脚 D、DW、DB、NS、PW、DYY 或 DGV 封装的任何逻辑器件。
封装 | 引脚 | CAD 符号、封装和 3D 模型 |
---|---|---|
SOIC (DW) | 24 | Ultra Librarian |
订购和质量
- RoHS
- REACH
- 器件标识
- 引脚镀层/焊球材料
- MSL 等级/回流焊峰值温度
- MTBF/时基故障估算
- 材料成分
- 鉴定摘要
- 持续可靠性监测
- 制造厂地点
- 封装厂地点