SIMPLELINK-WIFI-TOOLBOX
SimpleLink Wi-Fi 工具箱
SIMPLELINK-WIFI-TOOLBOX
概述
Wi-Fi 工具箱包提供了进行以下操作所需的全部功能:使用主机调试和监测 WLAN/低功耗 Bluetooth® 固件;执行射频验证测试;为监管认证测试执行预测试;调试硬件和软件平台的集成问题。
特性
- 无线电工具 - 无线电工具是一款在开发和监管认证过程中对 CC33xx 设计进行射频评估和测试的工具。通过手动将无线电设置为传输或接收模式,该工具可提供低级无线电测试功能。使用此工具可能需要熟悉并了解无线电电路理论和无线电测试方法的知识。
- INI composer - INI Composer 工具用于配置特定于 CC33xx 器件的射频参数和模式。该工具输出一个必须安装在嵌入式 Linux 文件系统内的 bin 文件。它还可在无线电工具中用于无线电测试和监管认证。
- 记录器 - 记录器用于从设备中捕获固件日志消息和协议事务。它可用于查看设备的内部数据和状态,以及与远程设备协议事务相关的信息。
- 要充分利用这些工具,需要连接 PC。要使用无线电工具启用 JTAG-to-USB 通信,我们建议使用 LP-XDS110ET LaunchPad™ 开发套件调试器或 TMDSEMU110-U XDS110 JTAG 调试探针。使用几乎任何类型的串口硬件 USB 都可捕获串口日志。我们建议使用 FTDI 串行线或 CC31XXEMUBOOST BoosterPack™ 插件模块。
下载
SIMPLELINK-WIFI-TOOLBOX — SimpleLink Wi-Fi Toolbox collection of tools to help development and testing of the CC33xx and CC35xxE Devices
支持的产品和硬件
产品
Wi-Fi 产品
硬件开发
评估板
SIMPLELINK-WIFI-TOOLBOX — SimpleLink Wi-Fi Toolbox collection of tools to help development and testing of the CC33xx and CC35xxE Devices
Windows Installer
Linux Installer
macOS Intel Ventura Installer
macOS Arm64 Ventura Installer
产品
Wi-Fi 产品
硬件开发
评估板
文档
Manifest
发布信息
SimpleLink Wi-Fi Toolbox is a comprehensive cross-platform development suite that delivers essential tools for streamlined development and rapid prototyping with the CC33XX and CC35XXE wireless connectivity solutions.
This is version 4.1.16 of the SimpleLink Wi-Fi Toolbox.
Previous release was 4.1.8
新增功能
- [Programmer] Enable rollback protection during Flash programming
- [Programmer] New capability for “Auto Flash Detection”
- [Programmer] “Flash Reset Type” is no longer required during Activation process
- [CLI] New and updated commands:
- For all CLI commands that required Flash type now can use “AUTO_DETECT” option.
- [All] Bugfixes and enhancements
- [General] Updated Toolbox User Guide
您可能需要的其他资源
SIMPLELINK-WIFI-SDK — SimpleLink Wi-Fi SDK for the CC35xxE Devices
支持的产品和硬件
产品
Wi-Fi 产品
硬件开发
评估板
SIMPLELINK-WIFI-SDK — SimpleLink Wi-Fi SDK for the CC35xxE Devices
产品
Wi-Fi 产品
硬件开发
评估板
发布信息
The SimpleLink™ Wi-Fi® SDK provides a comprehensive software toolkit for developing IoT applications on the CC35xxE family of wireless MCUs. This powerful SDK includes essential components like the Bluetooth® LE protocol stack supporting Bluetooth 5.4, Wi-Fi 6 with an included networking stack based on LwIP, and the FreeRTOS kernel and TI Drivers in one easy-to-use software package, along with example applications and exhaustive documentation. When used with TI’s SimpleLink Wi-Fi® CC35xxE LaunchPads, the SDK provides a complete development solution for IoT applications. This SDK is also available on GitHub at https://github.com/TexasInstruments/simplelink-wifi-sdk.
This is version 10.10.00.18 of the Wi-Fi SDK.
新增功能
- New device support CC35X1ET
- SDK New example applications: CC35XX OTA Example CC35XX Power measurement CC35XX BLE DTM CC35XX BLE controller
- Raw Wi-Fi CSI data available to application
- FWU Support for accept/reject API
- External coexistence 3-wire PTA Master
- WiFi AP Certifications
- Bug Fixes
CC33XX-QUICKTRACK-CONTROL-TOOL — CC33XX QuickTrack Control 应用是一款用于 Wi-Fi® 认证的 Wi-Fi 自动化测试工具
支持的产品和硬件
产品
Wi-Fi 产品
硬件开发
评估板
CC33XX-QUICKTRACK-CONTROL-TOOL — CC33XX QuickTrack Control 应用是一款用于 Wi-Fi® 认证的 Wi-Fi 自动化测试工具
CC33xx QuickTrack Control Tool Windows Installer
CC33xx QuickTrack Control Tool Linux Installer
产品
Wi-Fi 产品
硬件开发
评估板
文档
Manifest
发布信息
Click on the links in the table above to download. The CC33xx QuickTrack Control Tool is a Wi-Fi automation test tool utilized for Wi-Fi® Certification.
新增功能
- fixed paths
- fix wps APUT settings file
- wps pin checksum script
CC33XX-LINUX-MPU — CC33xx device driver source for MPUs running Linux OS.
支持的产品和硬件
产品
Wi-Fi 产品
硬件开发
评估板
CC33XX-LINUX-MPU — CC33xx device driver source for MPUs running Linux OS.
CC33xx Linux MPU Windows Installer
CC33xx Linux MPU Linux Installer
CC33XX Yocto Image for AM62p
CC33XX Yocto Image for AM62
CC33XX Yocto Image for AM335
产品
Wi-Fi 产品
硬件开发
评估板
发布信息
The CC33xx Linux MPU Software Package delivers components that enable engineers to develop connected applications on Texas Instruments Wi-Fi Companion-IC devices. The product is comprised of multiple software components and examples of how to use these components together. In addition, examples are provided to demonstrate the use of each functional area and each supported device and as a starting point for your own projects.
This CC33xx Linux MPU Software Package delivers components that enable operation of the Texas Instruments CC33xx Wi-Fi and BLE family of wireless transceivers on Linux platforms.
This is version **1.0.2.10** of the CC33xx Linux MPU Software Package
The version is a production quality release for 2.4/5Ghz devices
Previous release was 1.0.2.9
This is a release for TI’s CC33xx devices supporting Wi-Fi 6 and BLE 5.4.
Components version:
- FW version: 1.7.0.323
- Driver version: 1.7.0.239
- PHY version: 1.2.0.47.6.13.37.69
- RAM Bootloader version: 1.0.0.29
新增功能
- Wifi 6 disable via OTP fuse bits
- Improved SDIO in-band IRQ support in legacy MMC hosts
- TCXO mode - functional but not fully characterized and not supported as an operational mode
- Bug fixes
CC33XX-RTOS-MCU — CC33xx device driver for MCU and RTOS platforms
支持的产品和硬件
产品
Wi-Fi 产品
硬件开发
评估板
CC33XX-RTOS-MCU — CC33xx device driver for MCU and RTOS platforms
Linux Installer
Windows Installer
Source Zip
产品
Wi-Fi 产品
硬件开发
评估板
文档
Manifest
发布信息
This CC33xx RTOS MCU Software Package delivers components that enable engineers to develop applications on the Texas Instruments CC33xx Wi-Fi devices and Sitara family of microcontrollers (MCU).
This software toolkit provides the drivers for CC33xx devices to be used with a Real-Time Operating System (RTOS) on a microcontroller.
This is version R8 of the CC33xx RTOS MCU Software Package.
新增功能
- Fixed issue - Connection with PMF doesnt send deauth frame secured
- Feature Enhancement: One-Shot Channel List Scanning - Added ability to limit Wi-Fi scans or connections to a specific, user-defined channel list.
- Use WLAN_SET_LISTED_CHANNELS_FOR_SCAN with Wlan_Set to define your desired channels.
- This configuration is a one-time operation. Subsequent scans or connections will automatically default back to scanning all channels.
- To manually clear the list, provide a NULL pointer to the Wlan_Set operation.
- Various code cleanup