MMWAVE-L-SDK
适用于 xWRL1432、xWRL6432、xWRL6844 和 xWRL6843 的软件
MMWAVE-L-SDK
概述
毫米波低功耗软件开发套件 (SDK) 是一个软件包集合,支持在我们的低功耗毫米波传感器上进行应用评估和开发。此工具包括支持客户设计需求的 MMWAVE-L-SDK 和 MMWAVE-L-SDK-6 配套包。
MMWAVE-L-SDK 和 MMWAVE-L-SDK-6 是用于毫米波检测产品系列的统一软件平台,不仅设置简单,还可实现开箱即用的快速评估和开发。MMWAVE-L-SDK 和 MMWAVE-L-SDK-6 是客户应用开发所需的低功耗基础软件包,包括构建块、演示和示例。
汽车类演示应用包括为存在和运动、车内乘员检测、脚踢开启和泊车辅助量身定制的应用。
工业类演示应用包括为存在和运动、手势识别、人员跟踪和分类、液位感应等量身定制的应用
特性
- 构建块
- 完整驱动程序可用性(集成了驱动程序包)
- 用于执行各种器件低功耗模式的电源管理框架
- 编程模拟前端 (AFE) 的分层方法
- Arm® Cortex®-M4F 处理器支持 FreeRTOS™ 和非 RTOS
- 演示和示例
- 基于 FreeRTOS 的演示
- 低功耗可视化工具 GUI
- 易于配置的开箱即用演示
- 在演示中展示占位检测、点云和基准测试数据
- 开箱即用演示与电源管理框架集成,可使用特定于用例的超低功耗模式运行器件
- 配置文件针对常见的最终用户场景进行了调整,例如对运动的敏感度
- 工具
- Code Composer Studio™ 集成式开发环境 (IDE) (CCSTUDIO)
- 用于系统代码生成的系统配置工具 (SYSCONFIG)
下载
MMWAVE-L-SDK — mmWave SDK for xWRL6432, IWRL6432AOP, IWRL6432W and xWRL1432
支持的产品和硬件
产品
工业毫米波雷达传感器
汽车毫米波雷达传感器
硬件开发
评估板
MMWAVE-L-SDK — mmWave SDK for xWRL6432, IWRL6432AOP, IWRL6432W and xWRL1432
Windows Installer for the 05.05.04.02 SDK
Linux Installer for the 05.05.04.02 SDK
产品
工业毫米波雷达传感器
汽车毫米波雷达传感器
硬件开发
评估板
文档
Manifest for the 05.05.04.02 SDK
发布信息
- Building blocks
- Integrated driver packages.
- Power management framework to exercise different device low power modes .
- Layered approach to programming analog front end (AFE).
- FreeRTOS™ and no-RTOS support on Arm® Cortex®-M4F processor
- Demonstrations and examples
- FreeRTOS-based demos.
- Out-of-box demo with easy configurability via low power visualizer GUI.
- Out-Of-box demo integrated with the power management framework to operate the device in the lowest power mode possible for the use-case.
- Representation of “motion detect ” , "point cloud" and benchmarking data from demo via low power visualizer GUI.
- Profiles tuned to common end-user scenarios, such as sensitivity to motion.
- Tools
- Code Composer Studio™ integrated development environment (IDE) (CCSTUDIO).
- SysConfig for the system code generation.
新增功能
- Added Angle of Arrival Steering Vectors (AOASV) DPU for angle of arrival correction in IWRL6432 AOP devices
- Updated default profile configurations for various devices in Motion and Presence Detect (MPD) demo for better performance
- Added Range and Angle based SNR Compensation feature to Motion and Presence Detect demo
- Reduced the tracker configuration parameters taken via Command Line interface (CLI) for ease of use
- Added support to parse ADC data with sideband enabled in ADC data parsing scripts
- Bug fixes (Refer to Release notes in package for more details)
MMWAVE-L-SDK-6 — SDK for xWRL6844 Devices
支持的产品和硬件
产品
工业毫米波雷达传感器
汽车毫米波雷达传感器
硬件开发
评估板
MMWAVE-L-SDK-6 — SDK for xWRL6844 Devices
Windows Installer for the 06.01.00.05 SDK
Linux Installer for the 06.01.00.05 SDK
产品
工业毫米波雷达传感器
汽车毫米波雷达传感器
硬件开发
评估板
文档
Manifest for the 06.01.00.xx SDK
发布信息
Building blocks
- Integrated driver packages.
- Power management framework to exercise different device low power modes.
- Layered approach to programming analog front end (AFE).
FreeRTOS™ and no-RTOS support on Arm® Cortex®-R5F processor and TI digital signal processor C66x
Demonstrations and examples
- FreeRTOS-based Out-of-box demo with easy configurability via low power visualizer GUI.
- Out-Of-box demo integrated with the power management framework to operate the device in the lowest power mode possible for the use-case.
- FreeRTOS & no-RTOS based examples for various drivers.
Tools
- Code Composer Studio™ integrated development environment (IDE) (CCSTUDIO).
- SysConfig for the system code generation.
新增功能
- Improvements and Bug fixes (Refer Release Notes)
MMWAVE-UDFP-APPSW — uDFP Package for Low Power mmWave Radar Modules and Front End Device
支持的产品和硬件
产品
工业毫米波雷达传感器
硬件开发
评估板
MMWAVE-UDFP-APPSW — uDFP Package for Low Power mmWave Radar Modules and Front End Device
MMWAVE uDFP SW package for IWRL6432WMOD
产品
工业毫米波雷达传感器
硬件开发
评估板
发布信息
MMWAVE-uDFP SW for IWRL6432WMOD provides a wide range of features and configuration capabilities from Host Controller over SPI interface. Some configurations supported:
- Detection Sensitivity
- Motion Sensitivity
- Max range selection
- Region and Boundary Configuration
- Polar and Cartesian Co-ordinate Systems etc.
This package also contains mmWaveULink and ICD document that aids in integrating the modules to Host Application Software.
新增功能
- Visualizer performance improvements
- The Detection Sensitivity configuration has been expanded from 3 bits to 4 bits, increasing the number of supported sensitivity levels from 6 to 13
- Performance improvements for configurations
- Enhanced MPD logic to ensure smooth handling of zone state transitions
- Added UART Flash Device API to flash firmware images to the device's serial flash memory over UART
- Added error handling to log failures and halt the sensor when boot calibration is unsuccessful in the demo
- Fixed an incorrect FTDI API usage in ftdi_wrapper.c where FT_GetBitMode was being used instead of the proper MPSSE
- Fixed an issue where the point cloud data would occasionally remain static across consecutive frames, causing the visualization to appear frozen
- Fixed memory corruption in ml_uDFPStatusGetApi and ml_uDFPVersionGetApi where response buffer was cast to a larger struct type, causing stack overflow beyond the output struct
您可能需要的其他资源
MMWAVE-STUDIO-3G — mmWave studio GUI tools for third-generation parts (xWRLx432)
支持的产品和硬件
产品
工业毫米波雷达传感器
汽车毫米波雷达传感器
硬件开发
评估板
MMWAVE-STUDIO-3G — mmWave studio GUI tools for third-generation parts (xWRLx432)
产品
工业毫米波雷达传感器
汽车毫米波雷达传感器
硬件开发
评估板
文档
发布信息
mmWave Studio GUI is designed to characterize and evaluate TI mmWave sensor devices. This package includes the GUI, associated tools and firmware for the performance evaluation of TI mmWave sensor devices. For more information please refer to the MMWAVE Studio User Guide and Release note.
This version supports the following device variants - AWRL6432, IWRL6432, AWRL1432 and IWRL1432.
MMWAVE-STUDIO-XWRL68XX — mmWaveStudio for 3rd generation xWRL68xx devices.
支持的产品和硬件
产品
工业毫米波雷达传感器
汽车毫米波雷达传感器
硬件开发
评估板
MMWAVE-STUDIO-XWRL68XX — mmWaveStudio for 3rd generation xWRL68xx devices.
产品
工业毫米波雷达传感器
汽车毫米波雷达传感器
硬件开发
评估板
文档
发布信息
mmWaveStudio GUI is designed to characterize and evaluate TI mmWave sensor devices. This package includes the GUI, associated tools and firmware for the performance evaluation of TI mmWave sensor devices. For more information please refer to the mmWaveStudio user guide and release notes. mmWaveStudio 4.3 is designed to support TI 3rd generation low power devices like xWRL68xx. The mmWave DFP APIs for these devices are brand new and this version of mmWaveStudio supports only these 3rd generation device APIs.
新增功能
- Support for TI's 3rd generation low power mmWave sensors - xWRL68xx.
RADAR-TOOLBOX — Radar evaluation and development support package with example projects, documentation and tools
支持的产品和硬件
产品
工业毫米波雷达传感器
汽车毫米波雷达传感器
硬件开发
参考设计
评估板
RADAR-TOOLBOX — Radar evaluation and development support package with example projects, documentation and tools
产品
工业毫米波雷达传感器
汽车毫米波雷达传感器
硬件开发
参考设计
评估板
发布信息
The Radar Toolbox demonstrates the capabilities of TI's mmWave radar sensors through software demos, examples, source code and documentation. It supports the xWRx843, xWRLx432, xWRL68xx and xWR29xx families of mmWave radar devices. It is intended to be used as a companion package with the device's corresponding SDK (typically MMWAVE-SDK3, MMWAVE-MCUPLUS-SDK, MMWAVE-L-SDK-5 or MMWAVE-L-SDK-6) to demonstrate specific demos and features.
新增功能
- New Examples: AWRL6432 Child Presence Detection, AWR1432 Kick-to-Open in the Rain IWRL6432 Capon 2D People Tracking, IWRL6844 People Tracking, IWRL6432 Sleep Monitoring, AWR2x44P Safety Demo
- New Features: AWRL6844 In-Cabin Demo supports LVDS, 1D Sensing Supports 4096 Point FFT
- Tools: Updates to Applications Visualizer, Rename AWRL6844 InCabin GUI to Low Power InCabin GUI
- Documentation: New AWR294x to AWR2x44P Migration Guide
- Bug Fixes: Elevation Estimation bug fix for xWRx432
RADAR-ACADEMY — mmWave Radar Academy
支持的产品和硬件
产品
工业毫米波雷达传感器
汽车毫米波雷达传感器
硬件开发
评估板
RADAR-ACADEMY — mmWave Radar Academy
产品
工业毫米波雷达传感器
汽车毫米波雷达传感器
硬件开发
评估板
发布信息
New Modules
- Selecting the Right Radar Device -> Security Features Overview Provides a high-level overview of the security features available with TI mmWave radar devices
- These security features determine the type of application boot flow that is followed by that device
- Radar Algorithms -> Motion and Presence Detection In-depth look at the commonly used motion/presence detection state machine
- Provides context on how the state transitions work and how the algorithm can be configured for various applications